Post Go back to editing

How to read ADS7-V2 DUT 12V current

Thread Summary

The user inquired about programmatically reading the current to the DUT on the ADS7-V2 board using the ADM1178 hotplug controller connected to PMU_SDA and PMU_SCL. The final answer indicated that ADI does not provide software for these boards, but the hardware connections are in place for I2C communication. The user needs to send a 0x05 command to address 0xE4 and read back 3 bytes to poll the current.
AI Generated Content

On the ADS7-V2 board, there's a U10 (an ADM1178 hotplug controller) that handles the overcurrent protection on the 12V supply to the FMC connector.

That device is hooked up to PMU_{SDA, SCL} which then goes through a translator to the Blackfin and the FPGA.

Is there any API access to programmatically read the current going to the DUT?

...all the hardware and connections are there, it's just a matter of sending 0x05 (Command: I_CONT | V_CONT) to Addr 0xE4 and reading back 3 bytes...just need the C# assembly and code snippet to either do the I2C write/read myself, or just something where I can poll the current