Post Go back to editing

AD9102 Trigger and UPDATE bit (0x1D)

Thread Summary

The user encountered issues generating a sine wave from the AD9102 DAC after configuring registers from an example file and manually triggering the device. The solution involved setting the RUN bit in the PAT_STATUS register (Register 0x1E) to 1, which resolved the SPI communication and allowed the sine wave to be generated. Key registers for AD9102 configuration and troubleshooting were also discussed.
AI Generated Content

Hello everybody,

tried to send the registers which are in the example6.regval to FPGA, after that, I sent 0x01 to register 0x1D and then set Trigger high and low. But I have no Sine wave from DAC.

1- Should I repeat UPDATE bit (0x1D) for the trigger as well?

2- Is any specific time for trigger needed?

3- Is any specific time for UPDATE bit (0x1D) needed?

4- For Sine wave from DDS, should I write some data into the RAM? 

5- How can I read the sent data (from FPGA) through AD9102 software?

Regards,

Akbar

Edit Notes

DDS
[edited by: akbar at 2:54 PM (GMT 0) on 30 Apr 2019]
Parents
  • Hello Akbar,

    1-4: no

    5: click on the "Register_Contents" tap at the bottom of the GUI.

    Regards,

    Will

  • Dear Will,

    after loading example6.regval, trigger high and low is done by "write active tab". 

    1- What does do the "write active tab" ? Which register and bit are going to be changed?

    2- Is the example6.regval a specific configuration for using the eval-Board and GUI ? 

    Was it a proper decision using the example6.regval configuration to communicate between FPGA and DAC ? (I did the same, but no output Sine wave)

    Regards,

    Akbar

  • Yellow is SCLK

    0x02:

    0x07:

    and 0x7F:

    0x0E:

    0x0B:

    0x0C, 0x0B, 0x0A, 0x09:

    Trigger is high, after 2ms is low:

    Here the Yellow is Trigger.

  • Dear Will,

    as I mentioned previously,

    1- I copied the registers from "example6.regal" and sent to AD9102,

    2- due to unsuccessful result (sine wave), I only tried to send only 33 registers of the whole "example6.regal".

    Consequently, it would be greatly appreciated

    3- if you check these 33 registers and let me know whether they are correct or not:

    33 registers are:

    x"0000",   data = x"0000", 
    x"0001",   data = x"0E00",  
    x"0002",   data = x"0000",  
    x"0003",   data = x"0000",  
    x"0007",   data = x"4000",  
    x"0008",   data = x"0000",  
    x"000C",   data = x"1F00",  
    x"000D",   data = x"0000",  
    x"000E",   data = x"0000",  
    x"001D",   data = x"0000",  
    x"001E",   data = x"0000",  
    x"001F",   data = x"0000",  
    x"0020",   data = x"000E",  
    x"0025",   data = x"0000",  
    x"0027",   data = x"1232",  
    x"0028",   data = x"0111",  
    x"0029",   data = x"0200",  
    x"002B",   data = x"0101",  
    x"002C",   data = x"0003",  
    x"002D",  data = x"0000",  
    x"0031",   data = x"0000", 
    x"0035",   data = x"4000",  
    x"0037",   data = x"7E00",  
    x"003E",   data = x"0750",  
    x"003F",   data = x"7500",  
    x"0043",   data = x"0000",  
    x"0044",   data = x"0002",  
    x"0045",   data = x"0000",  
    x"0047",   data = x"0000",  
    x"005C",   data = x"0FA0",  
    x"005D",   data = x"0000",  
    x"005E",   data = x"0000",  
    x"005F",   data = x"7FFF" 

    x"001D",   data = x"0001", 

    By the way,

    4- reminder:

    the goal is to generate sine, triangle and square wave with AD9102. So, I have generated them using AD9102 Evaluation Board. 

    Now, I must do the same, generating sine, triangle and square wave  but sending registers from FPGA to AD9102.

    Regards,

    Akbar

  • Dear Akbar,

    The registers are double buffered, and they don't get updated until you write 0x1 to the RAMUPDATE register. Thus you can't read them back immediately.

    Regards,

    Will

  • Dear Will,

    Thank you for the reply, yes, for sure I write 0x1 to the RAMUPDATE register. So I did.

    Refering to your previouse responses in this topic, I write 0x1 to the RAMUPDATE register immediately after writing last register, then I read 128 registers back.

    Regards,

    Akbar

  • We have already talked about RAMUPDATE.

  • That is good. Although that is not the case that you showed in the plots yesterday. In those plots you read back immediately after write. Is the read back still wrong after you write RAMUPDATE?

    Regards,

    Will

  • Dear Will,

    the readback looks strange, maybe wrong.

    reading back these registers are following:

    I do not write to 0x0A, 0x0B and 0x0C, but readback is "1F0A", refering to "example6.regal" they should be "1F0A", thus it's ok.

    For 0x09, I write "1F0A", readback is "1F00", thus is not ok.

    For 0x07, I write "4000", but readback is "0000". So is not ok.

    Regards,

    Akbar

  • Dear Akbar,

    Many of the registers are for AD9106 and not applicable for AD9102. They include Reg0x09, 0x0A and 0x0B. Reg0x09 and 0x0C are legitimate, and you read back the default, so it appears that you didn't write the registers successfully.

    The data sheet said reg0x09 defaults to 0x000A. I check the eval board I have and that is incorrect, the default read back 0x1F0A. Sorry for the datasheet error.

    Regards,

    Will

  • Dear Will,

    furtheremore, refering to your suggestion, I set CS high after each address (Write command + address + data).

    Should I set a delay like this?

    The 32-bit data is transmitted by "CS low => delay => 16-bit address (SPI_CLK on) => delay => 16-bit parameter (SPI_CLK on)  => delay => CS high".

    https://ez.analog.com/data_converters/high-speed_dacs/f/q-a/22647/ad9102-fpga-communication/326571#326571

    Regards,

    Akbar

  • Sure. Replicating what the micro-controller does would be a great starting point.

    Regards,

    Will

Reply Children