Post Go back to editing

AD9102 Trigger and UPDATE bit (0x1D)

Thread Summary

The user encountered issues generating a sine wave from the AD9102 DAC after configuring registers from an example file and manually triggering the device. The solution involved setting the RUN bit in the PAT_STATUS register (Register 0x1E) to 1, which resolved the SPI communication and allowed the sine wave to be generated. Key registers for AD9102 configuration and troubleshooting were also discussed.
AI Generated Content

Hello everybody,

tried to send the registers which are in the example6.regval to FPGA, after that, I sent 0x01 to register 0x1D and then set Trigger high and low. But I have no Sine wave from DAC.

1- Should I repeat UPDATE bit (0x1D) for the trigger as well?

2- Is any specific time for trigger needed?

3- Is any specific time for UPDATE bit (0x1D) needed?

4- For Sine wave from DDS, should I write some data into the RAM? 

5- How can I read the sent data (from FPGA) through AD9102 software?

Regards,

Akbar

Edit Notes

DDS
[edited by: akbar at 2:54 PM (GMT 0) on 30 Apr 2019]
Parents Reply Children
  • Dear Akbar,

    For the trigger you want to make sure that jumper jp1 is open.

    The way you write the SPI, you want to bring CS_B high after writing reg0x0, and low again before writing reg0x1, and leave it low for the remainder of the SPI writes.

    If the SPI writes were not successful, you may also want to try writing each register separately (CS_B low, command, data, CS_B high).

    Regards,

    Will

  • Dear Will,

    surprised hearing that!

    You suggest "bring CS_B high after writing reg0x0, and low again before writing reg0x1, and leave it low for the remainder of the SPI writes."

    So why it has not been mentioned in the datasheet? Or is it a suggestion in this case?

    Regards,

    Akbar

  • Dear Akbar,

    The datasheet did mention that but not in great detail. According to page 18 of the datasheet, "The SPI port automatically increments the register address if CS_B stays low beyond the first data-word allowing writes to or reads from a set of contiguous addresses." If you don't bring CS-B high after writing reg0x0, it may interpret the next write command as data for reg0x1.

    Since reg0x0 is the configuration register, it is a good idea to finish the write by bring CS_B high, before proceeding to other registers.

    Regards,

    Will

  • Dear Will,

    Thank you for your reply.

    According to page 18 of the datasheet and as I understood, I brought CS_B low and kept it low, sent '0' [15] through SDIO as write command and '0' [14:0] as the address of Reg0x00. Then I sent the second byte '0' as data [15:0].

    After that, for the second register and second data (Reg 0x01 to 0x7F), I did not send the next address, because SPI port automatically increments the register address if CS_B stays low.

    Finally, for RAMUPDATE, Address 0x1D, I brought CS_B low, sent write command, address of Reg0x1D [14:0], then 0x01 as data for Reg0x1D.

    Regards,

    Akbar

  • Dear Akbar,

    I think what you are doing is fine. Just make sure that you can read back the correct values. Except the RAMUPDATE bit of course, since it is self clearing.

    Regards,

    Will

  • Dear Will,

    Thank you again for your reply.

    To Readback:

    1- can I read immediately after sending last data?

    Should I consider spesific time and then send the read command?

    2- should I follow same procedure? (CS_B low, first address, data, CS_B high, again CS_B low and so on...).

    Regards,

    Akbar

  • Dear Akbar,

    1, You want to do it after you write the RAMUPDATE bit and bring CS_B high.

    2. Yes.

    Regards,

    Will

  • Dear Will,

    I did following:

    CS_B low, first address, data, CS_B high, again CS_B low and so on... for every address, finally Readback was sucssefull but still I have not any out put signal.

    Regards,

    Akbar

  • Dear Akbar,

    I am sorry to hear that.

    The register values that you read back after you wrote through FPGA, are they the same as the values that you read back (by clicking on Register_Contents tab) before you modified the board? How did you apply the trigger_B signal?

    Regards,

    Will

  • Dear Will,

    as far as I remember, they were the same, but I am not 100% sure. I will let you know on Monday.

    1- Referring to your suggestion, jumper jp1 is open and I have connected the TP30 directly to the Trigger port.

    2- Actually, with the logic (FPGA), the trigger is high as default. I don't know whether default hight is correct? 

    So I set it high again (or keep it high again) not after one clock cycle, but only a few u sec, then low and again a delay, after that Readback is executed.

    Regards,

    Akbar