Hello everybody,
tried to communicate from FPGA to AD9102 via SPI and after transmission of values (which are in the example6.regval), I do write a 1 to the UPDATE bit in the "RAMUPDATE" register. But I can not have any sine wave (no generated wave).
1- Is the trigger missed? (In the software, there is a trigger option called "Trigger_PIC". So how can I trigger it via FPGA?)
Already tried to trigger via TP30, but unsuccessful.
or
2- Is the UPDATE bit in this case wrong?
Regards,
Akbar
Tp30
[edited by: akbar at 8:27 PM (GMT 0) on 25 Apr 2019]