| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Open | |
AD9102
Production
The AD9102 TxDAC and waveform generator is a high performance digital-to-analog converter (DAC) integrating on-chip pattern memory for complex waveform...
Datasheet
AD9102 on Analog.com
Trying to generate a Triangle wave with 78,125 KHz, 156,25 KHz, 312,5 KHz, 625 KHz, 1250 KHz, but I could not find any thing about the frequency for Triangle or Sawtooth wave.
I use the example2_4096_ramp.txt and example4.regval file, then I have changed:
the WAVE_SEL1 0x027[5:4] to 1
the SAW_STEP1 0x037[7:2] to 4.
So I have no idea how to change the frequency.

Actually, for the sin wave, I could easily change the frequency, by changing the DDS frequency in the DAC1 tab.
but for the Triangle wave, is vague.
Thank you in advance.
Hello,
Unfortunately the triangular waveform won't fit your need. The triangular waveform always ramp from positive full scale toward negative full scale and back in 1lsb step. To do what you want, you need to take multiple lsb steps. I suggest you use the on-chip RAM to store your waveform instead.
Regards,
Will
Hello Will,
thank u so much for the reply.
below lsb 1 step:

and this one, lsb 3 step:

1- Is that what u mentioned ?
As u mentioned, I used SRAM, to load my waveform (1 lsb and 3 lsb) and as Regval File, I use example1.regval to have triangular waveform.
2- How can I have Continuos triangle waveform ?
2.1- in this case, should I use the example6.regval ? (Actually, for the sin wave, I used the example6.regval and could easily change the frequency, by changing the DDS frequency in the DAC1 tab.)
3- Still I do not konw how to change the frequency !!!
Best regards,
Akbar
Hello Akbar,
Sorry for the delayed response! I was in a conference the last few days.
1. Right. But you can't have 3lsb step in the triangular waveform function, you can with SRAM.
2. You set PATTERN_RPT (reg0x1F[0]) to 0, and PATTERN_PERIOD (reg0x29) to the number of samples in the triangulare wave period.
3.You can either store multiple waveforms and change the start and stop address as you change frequency; or you can load a different waveform.
Regards,
Will
Hello again Will,
and thank u again for the reply.
I guess almost I did the same!!
Yes, the PATTERN_RPT (reg0x1F[0]) to '0', is clear, as it is mentioned in the data sheet, but regarding the 'PATTERN_PERIOD (reg0x29)', I thought when I choose to read from the SRAM (WAVE_SEL 0x0027[2:0] to '0'), I can not change the 'PATTERN_PERIOD (reg0x29)' anymore. But suddenly I varried the value to the number of samples in the SRAM, so there was useful, and then, I set the 'START_DLY 0x005C[15:0]' to '0'.
Regarding the 3rd answer,
I loaded different waveforms.
At the end, your answer was absolutely useful. There are enough post, about the same question in the forum, but they're not actually useful for me. at least, I could not find such a answer like yours.



0
16
32
48
64
80
96
112
128
144
160
176
192
208
224
240
256
272
288
304
320
336
352
368
384
400
416
432
448
464
480
496
512
528
544
560
576
592
608
624
640
656
672
688
704
720
736
752
768
784
800
816
832
848
864
880
896
912
928
944
960
976
992
1008
1024
1040
1056
1072
1088
1104
1120
1136
1152
1168
1184
1200
1216
1232
1248
1264
1280
1296
1312
1328
1344
1360
1376
1392
1408
1424
1440
1456
1472
1488
1504
1520
1536
1552
1568
1584
1600
1616
1632
1648
1664
1680
1696
1712
1728
1744
1760
1776
1792
1808
1824
1840
1856
1872
1888
1904
1920
1936
1952
1968
1984
2000
2016
2032
2048
2032
2016
2000
1984
1968
1952
1936
1920
1904
1888
1872
1856
1840
1824
1808
1792
1776
1760
1744
1728
1712
1696
1680
1664
1648
1632
1616
1600
1584
1568
1552
1536
1520
1504
1488
1472
1456
1440
1424
1408
1392
1376
1360
1344
1328
1312
1296
1280
1264
1248
1232
1216
1200
1184
1168
1152
1136
1120
1104
1088
1072
1056
1040
1024
1008
992
976
960
944
928
912
896
880
864
848
832
816
800
784
768
752
736
720
704
688
672
656
640
624
608
592
576
560
544
528
512
496
480
464
448
432
416
400
384
368
352
336
320
304
288
272
256
240
224
208
192
176
160
144
128
112
96
80
64
48
32
16
0
-16
-32
-48
-64
-80
-96
-112
-128
-144
-160
-176
-192
-208
-224
-240
-256
-272
-288
-304
-320
-336
-352
-368
-384
-400
-416
-432
-448
-464
-480
-496
-512
-528
-544
-560
-576
-592
-608
-624
-640
-656
-672
-688
-704
-720
-736
-752
-768
-784
-800
-816
-832
-848
-864
-880
-896
-912
-928
-944
-960
-976
-992
-1008
-1024
-1040
-1056
-1072
-1088
-1104
-1120
-1136
-1152
-1168
-1184
-1200
-1216
-1232
-1248
-1264
-1280
-1296
-1312
-1328
-1344
-1360
-1376
-1392
-1408
-1424
-1440
-1456
-1472
-1488
-1504
-1520
-1536
-1552
-1568
-1584
-1600
-1616
-1632
-1648
-1664
-1680
-1696
-1712
-1728
-1744
-1760
-1776
-1792
-1808
-1824
-1840
-1856
-1872
-1888
-1904
-1920
-1936
-1952
-1968
-1984
-2000
-2016
-2032
-2048
-2032
-2016
-2000
-1984
-1968
-1952
-1936
-1920
-1904
-1888
-1872
-1856
-1840
-1824
-1808
-1792
-1776
-1760
-1744
-1728
-1712
-1696
-1680
-1664
-1648
-1632
-1616
-1600
-1584
-1568
-1552
-1536
-1520
-1504
-1488
-1472
-1456
-1440
-1424
-1408
-1392
-1376
-1360
-1344
-1328
-1312
-1296
-1280
-1264
-1248
-1232
-1216
-1200
-1184
-1168
-1152
-1136
-1120
-1104
-1088
-1072
-1056
-1040
-1024
-1008
-992
-976
-960
-944
-928
-912
-896
-880
-864
-848
-832
-816
-800
-784
-768
-752
-736
-720
-704
-688
-672
-656
-640
-624
-608
-592
-576
-560
-544
-528
-512
-496
-480
-464
-448
-432
-416
-400
-384
-368
-352
-336
-320
-304
-288
-272
-256
-240
-224
-208
-192
-176
-160
-144
-128
-112
-96
-80
-64
-48
-32
-16
Dear Will,
two more questions:
4- If you see the waveforms, I guess I need to change the offset. What do u think?
5- As the highest value, I used 2048 for the samples. Is it possible to use 4096?
Actually, I loaded a waveform with the 4096 but did not work out correctly. Occurs Clipping.
Thank u for your consideration.
Regards,
Akbar
Hello Akbar,
4. By changing offset do you want to center it around VDD/2? Unfortunately you can't not do that without a external amplifier or transformer. The output is DAC current from VDD to VSS, thus the minimum output is VSS (when that current is zero).
5. The 12bit RAM data is signed, so it goes from -2048 to +2047.
Regards,
Will
Hello Akbar,
4. By changing offset do you want to center it around VDD/2? Unfortunately you can't not do that without a external amplifier or transformer. The output is DAC current from VDD to VSS, thus the minimum output is VSS (when that current is zero).
5. The 12bit RAM data is signed, so it goes from -2048 to +2047.
Regards,
Will
Hello Will,
thank you very much fpr your time and consideration.
Regards,
Akbar
Forgot to mention that for 4. you could also do AC coupling or resistive level shifting etc. In either case you need some kind of hardware modification.
Hello Will,
concerning the 4- offset, not only VDD/2, but maybe lower or even higher.
Does the DAC Digital Offset Register (DACDOF, Address 0x25) the same ?
Regards,
Akbar
Hello Akbar,
Adding a digital offset shifts one output up and the other down. You will need to reduce your swing to avoid clipping the waveform.
Regards,
Will