AD9866
Not Recommended for New Designs
The AD9866 is a mixed-signal front end (MxFE®) IC for
transceiver applications requiring Tx and Rx path functionality
with data rates up to 80 MSPS. Its...
Datasheet
AD9866 on Analog.com
I am testing the ad9866.But there is a question about RXSYNC.The ad9866 is configured as:mode=high(full-duplex),config=high,PWR_DWN=low,RESET=high.The spi is configured as default value(after S/W Reset).I receive the RX data but RXSYNC is always low or high.So what should I do?
Hello,Has anyone encountered this problem?
Assumed answered offline. Let us know if there are further questions.
Assumed answered offline. Let us know if there are further questions.