When using the AD9705 with the 1.25V internal reference what should be the voltage on the FS ADJ pin?
When using the AD9705 with the 1.25V internal reference what should be the voltage on the FS ADJ pin?
FS ADJ is the same voltage as REFIO. So if you use internal reference (1.025V not 1.25V) then FS ADJ is also about 1.025V. If you use external reference, it can go up to 1.25V.
We have been unable to see this behavior on our chip. We have tried three different chips. Two on our board, and one on a breakout. We are using the example circuit with the AD5620 shown in this circuit note. https://www.analog.com/media/en/reference-design-documentation/reference-designs/CN0156.pdf
Here is our circuit
We have been running the AD9705 in pin mode.
The REFIO is at 1.022V. We started with the vout of the AD5620 at zero or as close as it gets. It is at 16mv right now. We can change it over SPI. The FS ADJ just goes to whatever voltage we put out of AD5620. RSET is at 6.8k.
Is DAC_SLEEP/CSB at 0V?
Yes it is
Is Rset the resistor between AD5620 and AD9705? You said FS ADJ is same as VOUT at 16mV? Do you get anything from the DAC? If you set DAC_SLEEP/CSB to Vdd, does Vout change?
What value are the resistors around the transformer? what impedance is to the right of the transformer? What is OTCM set to?
RSET is between the two dacs. Yes, FS ADJ is the same. Nothing from the DAC. Vout does not change. The resistors around the transformer are DNI. Right of the transformer is a high Impedance buffer. OTCM is floating, nc.
Try connect OTCM to ground.
I guess the DNI resistors are either open or short as appropriate, as they can't be all open or all short.
With OTCM to ground FS ADJ and the REFIO are at 1.050. Still no output on the DAC however
That is good news! So FS ADJ went from 16mV to 1.05V is that right? That means there is right current flowing through Rset. What is the input data to 9705?
Hmm, how is that possible? I assume the center tap of the transformer is grounded. Can you sent a enlarged picture of the area around the transformer, and point out which resistors are open and which are short? BTW, you need SOME termination for the DAC, at least the resistor across the coil with center tap.
Hmm, how is that possible? I assume the center tap of the transformer is grounded. Can you sent a enlarged picture of the area around the transformer, and point out which resistors are open and which are short? BTW, you need SOME termination for the DAC, at least the resistor across the coil with center tap.
R95 is now populated with 22 ohm
And R85, R86 R91-94, R96? Where do you measure Iout?
R85,R86 short
R 91-94 open
R96 is now open
We have been measuring at pin 3 of transformer usually.
Try short out R92 and put populate R91 with 100ohm.
That did it. Thanks so much!
My pleasure. Glad to help!