AD9173
Recommended for New Designs
The AD9173 is a high performance, dual, 16-bit digital-to-analog converter (DAC) that supports DAC sample rates to 12.6 GSPS. The device features an 8...
Datasheet
AD9173 on Analog.com
I've used the AD9173 Eval FMC with both the USB interface in "standalone" mode, and on an KC705 HPC FMC. The "serial port configuration over SPI" works reliably, we have validated this. I am experiencing two curious behaviors which suggest maybe my eval board has bad silicon.
1- When I put the chip in DC test mode with the main NCO programmed at 1GHz, and the two amplitude registers set to 0x50ff, DAC0 will output the tone as expected, DAC 1 will not. However, if I setup the Channel NCO to output a tone, both DACs behave correctly. Is this normal behavior? This is behavior is consistent whether I use our own software or the FMC plugged into USB with ADI ACE.
2- We are using the DAC in dual JESD link mode. The PRBS test succeed, the link setup and stabilize. I get CGS, FS, CHECKSUM, and ILA bits set for the links and lanes in use. I have the proper JESD mode configured and when I poll registers 0x450 and on, it reports the proper settings from the JESD transmitter. When I run short_tpl test, it always passes... even when I program the check registers with a bad value! However, if I don't disable the test mode as described in step 9 of the data sheet on page 44 of the STPL test, it always fails, even with the right test pattern programmed. Furthermore, the chip will randomly not output data on DAC1 (or DAC0). All of the status regs (470-473) show a good link, and registers 4b0 - 4b7 show good links as well, and the sync out is solid high (view it on chips cope). We've run out of options. We are suspecting the silicon on the sample board may be bad. We would like to know if there is any status which we can read that ensures the DAC is streaming data on both ports? To remedy the problem, without reprogramming the device, we enter the PRBS test mode on the JESD links. Incidentally, both links show pass and 0 error count on all lanes, and when we return from the test, the DACs successfully stream data. We thought it might have to do with an overflow/underflow condition, so we even check the FIFO status bits, and they both show that we are neither empty nor full, so the DAC is definitely able to keep up with the data flow.
3- Some other observations: we are using physical lanes 4-7. 4 and 5 are link 0, with the crossbar sending them to logical lane 0 and 1 for link 0. Lanes 6 and 7 are mapped to logical lane 4 and 5 supplying lane 0 and lane 1 of link 1. Again, every register that we can think of that shows status suggest we have a working link. We just can't verify proper streaming. For our test, the main NCO for each DAC is set to 1GHz, and the Channel NCO FTW is set to 0. However, we have both main and channel NCOs configured to use the NCO because we have complex interpolation (24x) enabled (JESD MODE 3 with 8x and 3x interp for main and channel), so we are consistent with the data sheet (reg 112 bit 3 and reg 130 bit 6 are set) and we can verify proper behavior (when the chip is working). From the init, the boot loader successful flag is set (reg 705), the DAC PLL is locked (register 7b5), the DAC DLL is locked (register c3), DACs all complete calibration (register 52), the JESD mode is valid (register 110), the FTWs load (register 113), and SERDES PLL lock (register 281).
Incidentally, all register addresses are in hex. Just to clarify.
Please advise on how to determine the silicon is behaving as it should. Thank you!
To keep things simple, lets try getting the NCO-only mode working reliably. You should be able to get two NCO tones, one from DAC0 and one from DAC1. We had done this in the past many times...
In ACE, you can setup two main NCO only if a dual-link is selected. for the reason I mentioned above - if in single-link, the DAC1 datapath is left powered-down.
The red flag here is the intermittent behavior. How are you clocking the DAC? Direct clock or using the DAC PLL? I would expect intermittent issues If there is excessive phase-noise (jitter), or if the clock wanders (e.g. over temp), or if the clock input power is low. Note that on the EVB we have a balun the doesn't quite reach >8-9GHz (attempting to cover some 12GHz of bandwidth on the EVB, at a reasonable cost), so if bypassing the DAC PLL you may need some 16dBm to overcome the balun roll-off at 12GHz.
Would you have a spectrum analyzer accessible? Keysight's PXA or similar.
Noted on Examples #1 and #2. For #2 (Regarding ACE and the extra write), ACE was coded to have modular subroutines, so assuming a current DAC state is impossible. Writes are redundant in many cases. Many of them to page and re-page the correct DAC - the cost of object-oriented programming I suppose.
For #1 I'd need to check. BER readback registers for the PRBS tests, for example, are PASS by default, and need to be reset before the start of each test, to show 0xFF. So PASS until FAIL, and the bits are sticky.
To keep things simple, lets try getting the NCO-only mode working reliably. You should be able to get two NCO tones, one from DAC0 and one from DAC1. We had done this in the past many times...
In ACE, you can setup two main NCO only if a dual-link is selected. for the reason I mentioned above - if in single-link, the DAC1 datapath is left powered-down.
The red flag here is the intermittent behavior. How are you clocking the DAC? Direct clock or using the DAC PLL? I would expect intermittent issues If there is excessive phase-noise (jitter), or if the clock wanders (e.g. over temp), or if the clock input power is low. Note that on the EVB we have a balun the doesn't quite reach >8-9GHz (attempting to cover some 12GHz of bandwidth on the EVB, at a reasonable cost), so if bypassing the DAC PLL you may need some 16dBm to overcome the balun roll-off at 12GHz.
Would you have a spectrum analyzer accessible? Keysight's PXA or similar.
Noted on Examples #1 and #2. For #2 (Regarding ACE and the extra write), ACE was coded to have modular subroutines, so assuming a current DAC state is impossible. Writes are redundant in many cases. Many of them to page and re-page the correct DAC - the cost of object-oriented programming I suppose.
For #1 I'd need to check. BER readback registers for the PRBS tests, for example, are PASS by default, and need to be reset before the start of each test, to show 0xFF. So PASS until FAIL, and the bits are sticky.