Post Go back to editing

Programming and Controlling ADS7-V2 with AD9164 Daughter Card with MATLA

Hello,

I have downloaded DPG Downloader Version 1.3.77.154 and ACE Version 1.23.3085.1388.

The ADS7-V2 is Rev D and the 9164 eval board is also Rev D.

I am trying to control the output using MATLAB with the instructions found here:
https://wiki.analog.com/resources/eval/dpg/matlab-ads7

However, I am running into an the following AD9162Setup.m:

Unable to resolve the name AnalogDevices.DPG.Interfaces.SubclassMode.Subclass1

jesd204Core.Tx.Subclass = AnalogDevices.DPG.Interfaces.SubclassMode.Subclass1;

I am not really sure where to proceed from here.

Parents
  • Hi,

    It looks like the script would need updated for the latest version of DPG Downloader (1.3.77.154). You can inspect the DPG Interfaces DLL with an object browser to relocate relevant classes.

    The particular item can be fixed with:
    AnalogDevice.DPG.Interfaces.JESD204CoreInterface.SubclassMode.Subclass1

    I suspect you'll run into more issues, unfortunately.

Reply
  • Hi,

    It looks like the script would need updated for the latest version of DPG Downloader (1.3.77.154). You can inspect the DPG Interfaces DLL with an object browser to relocate relevant classes.

    The particular item can be fixed with:
    AnalogDevice.DPG.Interfaces.JESD204CoreInterface.SubclassMode.Subclass1

    I suspect you'll run into more issues, unfortunately.

Children
  • Hello,

    I also encountered the same issue. The only difference is I'm using an AD9174 board but I assume there won't be much difference. As you suggested, I replaced 'AnalogDevices.DPG.Interfaces.SubclassMode.Subclass1' with 'AnalogDevice.DPG.Interfaces.JESD204CoreInterface.SubclassMode.Subclass1' in the sample script, but it still showed 'unable to resove the name'. Do you have any idea of it? Did I do it in the wrong way?

    Thanks