Post Go back to editing

latency of the AD9777,5,3 DAC family

What is the latency of AD9777,AD9775 and AD9773 16,14 and 12 bit DACs

The answer is shown in the table below.

AD977X Latency Table
Interpolation Rate Modulation Rate Stage 1 Latency Stage 2 Latency Stage 3 Latency Modulator Latency Total Latency
2 1 56 0 0 0 56
2 2 56 0 0 20 76
2 4 56 0 0 22 78
2 8 56 0 0 21 77
4 1 112 34 0 0 146
4 2 112 34 0 20 166
4 4 112 34 0 22 168
4 8 112 34 0 21 167
8 1 224 68 24 0 316
8 2 224 68 24 20 336
8 4 224 68 24 22 338
8 8 224 68 24 21 337
Note: All latencies expressed in multiples of the DAC update rate, fDAC
Parents Reply Children
No Data