Post Go back to editing

AD9773 : default values of register

Hello,

I have a question about AD9773 from our customer.
He is asking us the default values about all registers.
The registers are being described in P.18 to 21 of the datasheet (Rev.D).
Default values are indicated in some registers, but there are also registers in which defaults are not indicated.

Could you indicate the default value of following register ?


Address    Bit
  02h     [7:6]
  03h     [1:0]
  04f     [2:1]
  05h     [7:0]
  06h     [3:0]
  07h     [7:0]
  08f     [1:0]
  09h     [7:0]


Best regards,
ysuzuki

  • Hello ,

    I'm sorry, I made typing mistake.

    I modified it to make correct.

    Address    Bit
      02h      [7:6]
      03h      [1:0]
      04h      [2:1]
      05h      [7:0]
      06h      [3:0]
      07h      [7:0]
      08h      [1:0]
      09h      [7:0]

    Best regards,
    ysuzuki