AD9164 - Achieving Deterministic Latency

I am trying to obtain deterministic latency between the AD9164 and a Xilinx UltraScale+ FPGA using the Xilinx JESD204B core. I can establish a link between the devices and reliably transfer data, but the latency through the device changes from POR to POR. Note I am running both the DAC and Xilinx Core in Continuous sync mode. The JESD interface is configured as follows.

Data rate: 4.8GHz

Lane rate: 12GHz

PCLK rate: 300MHz

Frame rate: 1.2GHz

M=1

L = 8

F = 1

S = 4

I believe that my clock relationships are correct and that I am meeting the Setup/hold requirements for SYSREF but I cant see the clocks right at the part. I can only observe at the PLL generating both DCLK and SYSREF clocks.  Is there anyway to verify using registers inside the part?

To measure the latency through the interface, I have a data generator inside the FPGA that I am using to generate a 300MHz sine wave. Until enabled, the data generator outputs zeros and when enabled generates a 300MHz sine wave. The enable used to start the generator is output with the data and I am using it to measure the delay from the start of data transmission into the JESD transmitter until the data is output from the DAC. I am also reading the the SYSREF_PHASEx  and SYNC_LMFC_STATx registers with each transfer. These are the latencies I am seeing from POR to POR and the SYSREF_PHASE for each:

SYSREF PHASE         Delay

       0xF80                  156.2nS

       0xFC0                  160.0nS

       0xFC0                  136.8nS

       0xF80                   136.8nS

       0xF00                   136.8nS

       0xF80                   136.6nS

       0xF80                   139.8nS

       0xFE0                   137n

Parents
  • To eliminate the variability caused by SYSREF phase as reported by registers 0x037 and 0x038. I collected the POR-to-POR delays for a single SYSYREF phase. What I observed is that for any of the 4 SYSREF phases the POR-to-POR delays obtains are always one of eight values. Each is separated by 1 PCLK; the total delay span is equal to 8 PCLKs. Other than the 1 the  I am observing to a single sysref phase as reported by registers 0x038 and 0x037 what I found is that the POR-to-POR delays observed  fall into 8 distinct bins; each separated by 1 PCLK and the total delay span is 8 PCLKs. If I factor out the skew caused by the SYSREF phase, the delays are the same for all 4 possible SYSREF phases. It would appear as though a divide by 4 and a divide by 2 counter somewhere in the SERDES clock circurty is not being reset or the PLL is not locking up correctly. But the state of the PLL_STATUS register (0x281) indicates that the PLL is locked and all is well.

    If I leave LMFC_DELAY and LMFC_VAR registers (0x304 and 0x306) programmed to their reset states and monitor the DYN_LINK_LATENCY register (0x302) the value reported after each POR-to-POR it can be used to determine which of the 8 delays that will occur. Unfortunately it is only correct about 75% of the time. The other 25% the delay is off by 1 PCLK.

    It is interesting that there is significant correlation to the observed delays to both PCLK and LMFC_DELAY and this must all mean something. I could definitely use some help from Analog Devices to solve this issue.

Reply
  • To eliminate the variability caused by SYSREF phase as reported by registers 0x037 and 0x038. I collected the POR-to-POR delays for a single SYSYREF phase. What I observed is that for any of the 4 SYSREF phases the POR-to-POR delays obtains are always one of eight values. Each is separated by 1 PCLK; the total delay span is equal to 8 PCLKs. Other than the 1 the  I am observing to a single sysref phase as reported by registers 0x038 and 0x037 what I found is that the POR-to-POR delays observed  fall into 8 distinct bins; each separated by 1 PCLK and the total delay span is 8 PCLKs. If I factor out the skew caused by the SYSREF phase, the delays are the same for all 4 possible SYSREF phases. It would appear as though a divide by 4 and a divide by 2 counter somewhere in the SERDES clock circurty is not being reset or the PLL is not locking up correctly. But the state of the PLL_STATUS register (0x281) indicates that the PLL is locked and all is well.

    If I leave LMFC_DELAY and LMFC_VAR registers (0x304 and 0x306) programmed to their reset states and monitor the DYN_LINK_LATENCY register (0x302) the value reported after each POR-to-POR it can be used to determine which of the 8 delays that will occur. Unfortunately it is only correct about 75% of the time. The other 25% the delay is off by 1 PCLK.

    It is interesting that there is significant correlation to the observed delays to both PCLK and LMFC_DELAY and this must all mean something. I could definitely use some help from Analog Devices to solve this issue.

Children