AD9957: FAQ

  • Created
  • Updated
Was this helpful?
  • 64 bit Windows compatibility

    Question There is an issue when trying to connect AD9957 evaluation board : USB port is not recognized by Windows 7 64 bits. Do you confirm? Is is possible to get updated driver? (USB chip on the…
  • AD9956: Run-time error 13

    Question I have a following problem with AD9956 evaluation board software. When the program successfully connects to the board on USB, I'm getting an error message : Run-time error '13' Type mismatch…
  • AD9957: maximum signal bandwidth

    Question In AD9957's datasheet, as figure 1 shown, the AD9957 output signal's bandwidth is about 10MHz. I want to know what the maximum signal bandwidth of AD9957 can process is. Answer The maximum…
  • AD9957_CCI overflow

    Question If we configure the 21st bit of CFR1 to 0, then the CCI_OVFL Pin was always high; If we configure the bit as 1, then the CCI won't overflow. In normal operation, should this bit be configured…
  • AD9957AD9910_Matched Latency Enable Bit

    Question I am using AD9957, the reference clock is 48MHz, the system clock is 960MHz, output 60MHz signal(Single Tone Mode), and met a problem. 1. When he configured "Matched Latency Enable " Bit as…
  • Can the AD9957 Evalboard and software generate CDMA modulation of the AD99957?

    Question Can the AD9957 Evalboard and software generate CDMA modulation of the AD99957? Answer In general, the AD9957 can produce any modulated signal that relies on a complex baseband component (I…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.