AD9786: FAQ

  • Created
  • Updated
Was this helpful?
  • AD9786: Current output voltage calculation

    Question I found a problem with one of my customers where AD9786 full scale output power under single tone test condition is only 3 dBm, much lower than the specified value 10dBm, so they would like…
  • AD9786: Propagation delay

    Question What is the dependency of the propagation delay and settling time of the AD9786? Answer Propogation delay is dependent on mostly digital filter configuration since each filter has its own group…
  • AD9786: Reset timing

    Question For our application we are using the DAC AD9786 as a straight DAC, that is, with the default settings. We are not using the SPI interface either. We want, however, to Reset the DAC each time…
  • AD9786: Thermal pad connection

    Question 1.) Pg 9 - Pin 2 is DNC Pg 47 - Pin 2 is labeled as LPF in the application circuit. 2.) Pg 55 - Must the thermal pad be connected to AGND or DGND? Answer 1) DNC = Do Not Connect My guess…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.