AD9734: FAQ

  • Created
  • Updated
Was this helpful?
  • AD9734: multichip SYNCHRONIZATION

    Question 1, I am using four AD9734s. Because DACCLK is divided by 2 to create DATACLK_OUT, the phase of DATACLK_OUT can be 0° or 180°, it's uncertain. As the red line shown (attache figure 1), the…
  • AD9734: Synchronize two DACs

    Question We are using two AD9734 DAC's for impementing wideband wireless backhaul modem analog frontend. Two DAC's used for synchronous transmission of two baseband channels. To sync the DAC's we enable…
  • Alias Frequencies

    Question I'd like a sine wave of 2.375 GHz, so the plan is to generate 375 MHz but as the sample rate is 1 Gsps, the aliases will appear at 625 MHz, 1.375 GHz, 1.625 GHz, 2.375 GHz 2.625 GHz and so…
  • Datasheet errors in the AD9736/5/4

    Question Question 1) Is the datasheet 288522419AD9734_5_6_0.pdf the latest version? There seem to be pinout errors on page 54 og 68. Question 2) What connections are reccommended for the 2 unused…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.