Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety

    Power limitations have always plagued process sensors, whether because of intrinsic safety requirements (safety achieved through power limitation) or because...

     

    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

    Latest Blogs

    • ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​
    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • -AD6676: FAQ
    • I noticed that it is possible to further reduce the full-scale input power requirements to the AD6676.  Is there any trade-offs that I need to be aware of when considering this option?
    • Operating AD6676 at  Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
    • What determines the AD6676’s full-scale input setting?
    • What is the STF response of a Σ-Δ ADC and why does it matter?
    • AD6676 Can you explain what the “Profile feature” is and why I it may be advantageous to use in some applications?
    • AD6676 What development tools are available?
    • AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
    • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    • AD6676 Why is the AD6676’s IF input resistance 60 ohms vs 50, 100 or even 200 ohms?
    • AD6676 Why isn't the noise floor of the AD6676 flat?
    • AD6676 I heard that Σ-Δ ADC’s can be driven into overload resulting in unstable behavior.  Is this true and should I be concerned?
    • Operating AD6676 at Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • +AD9560: FAQ
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?

An IF-sampling ADC typically refers to any ADC capable of digitizing an IF signal in its 2nd Nyquist zone (or higher) while still achieving sufficient dynamic range for the target application.   In a heterodyne or direct-sampling VHF receiver architecture, the IF-sampling ADC is just one of several components required in the IF strip to complete the signal chain.  Other components in support of the IF-strip may also include an IF SAW filter, digital-gain-amplifier, L-C “roofing” filter, ADC buffer amp, and clock generation IC. 

The AD6676 is called a wideband IF receiver subsystem because it integrates much of this functionality into a small 4.3mm x 5.0mm WLCSP package allowing it to directly interface to an RF-to-IF mixer via a simple low order L-C “roofing” filter resulting in considerable PCB area savings.   The continuous-time band-pass Σ-Δ ADC operates up to 3.2 GSPS thus “oversampling” the IF signal while providing very high dynamic range (NSD as low as -160 dBFS/Hz).  This attribute eliminates the need for an IF SAW filter (and subsequent IF gain stage) that serves as an aggressive anti-aliasing filter for a typical IF-sampling architecture.    Additionally, its low full-scale input power of -2 dBm (or less) allows considerable headroom to use its on-chip digital attenuator for AGC or level planning purposes.   In fact, RF-IF component line-ups operating off a 3.3 V supply become feasible (along with power savings) since the P1dB requirements of these components can be relaxed.  Digital integration also includes a QDDC with selectable digital decimation filters to provide 16-bit I/Q data transferred to the host over a JESD204B interface. Additional digital features facilitate fast AGC control, fast TDD power-down savings modes, and the ability of the Σ-Δ ADC to be quickly reconfigured in under 1 µsec to four different IF and bandwidth settings.  

In summary, the AD6676 is a re-configurable wideband IF receiver system that can enable some of the smallest, yet highest AGC-free dynamic range heterodyne or direct-sampling VHF radio receivers in the industry.

 

For more information, visit the AD6676 product page.

Tags: wideband_if high_speed_converter ad6676 high_speed_adc if_sampling_adc wideband_if_receiver_subsystem high_speed_analog_to_digital_converter Show More
  • Share
  • History
  • More
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved