Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety

    Power limitations have always plagued process sensors, whether because of intrinsic safety requirements (safety achieved through power limitation) or because...

     

    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

    Latest Blogs

    • ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​
    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents AD6676 Why isn't the noise floor of the AD6676 flat?
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • -AD6676: FAQ
    • I noticed that it is possible to further reduce the full-scale input power requirements to the AD6676.  Is there any trade-offs that I need to be aware of when considering this option?
    • Operating AD6676 at  Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
    • What determines the AD6676’s full-scale input setting?
    • What is the STF response of a Σ-Δ ADC and why does it matter?
    • AD6676 Can you explain what the “Profile feature” is and why I it may be advantageous to use in some applications?
    • AD6676 What development tools are available?
    • AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
    • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    • AD6676 Why is the AD6676’s IF input resistance 60 ohms vs 50, 100 or even 200 ohms?
    • AD6676 Why isn't the noise floor of the AD6676 flat?
    • AD6676 I heard that Σ-Δ ADC’s can be driven into overload resulting in unstable behavior.  Is this true and should I be concerned?
    • Operating AD6676 at Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • +AD9560: FAQ
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

AD6676 Why isn't the noise floor of the AD6676 flat?

I am looking at the noise spectral density (NSD) plots shown in NOMINAL PERFORMANCE characteristics of the datasheet and noticed that they are not flat and can vary depending on the AD6676 configuration.  Why?

 

The AD6676 includes a tunable continuous-time band-pass Σ-Δ ADC.  The very nature of this ADC architecture results in an NSD that is “shaped” rather than flat.  The degree of which the NSD is shaped is primarily dependent on the oversampling ratio (OSR = FADC/(2*BW) with a higher OSR resulting a flatter noise floor.  Other parameters that can influence the NSD (as well as signal frequency response) are listed in Table 7 of the datasheet and are referred to as User Specified Application Parameters.   Refer to the datasheet to learn how all these parameters impact the response of the Σ-Δ ADC.

Tags: wideband_if evaluation-system ad6676 high_speed_adc high_speed_converters if_sampling_adc wideband_if_receiver_subsystem high_speed_analog_to_digital_converter Show More
  • Share
  • History
  • More
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved