Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    Maximize Your Power Regulator: Key Considerations for Thermal Performance

    Power regulators with integrated switches deliver a compact, efficient way to supply power. Yet as modern circuits drive toward ever-higher power densities...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Understanding Voltage Domain Isolation in Field-Bus Systems

    By Christopher Nunes In the world of industrial communication, mastering voltage domain isolation is the key to building safer, smarter systems. Last...

     

    Ethernet-APL’s Impact on Functional, Intrinsic, and Cyber Safety

    Power limitations have always plagued process sensors, whether because of intrinsic safety requirements (safety achieved through power limitation) or because...

    Latest Blogs

    • Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression
    • ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​
    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • -AD6676: FAQ
    • I noticed that it is possible to further reduce the full-scale input power requirements to the AD6676.  Is there any trade-offs that I need to be aware of when considering this option?
    • Operating AD6676 at  Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
    • What determines the AD6676’s full-scale input setting?
    • What is the STF response of a Σ-Δ ADC and why does it matter?
    • AD6676 Can you explain what the “Profile feature” is and why I it may be advantageous to use in some applications?
    • AD6676 What development tools are available?
    • AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
    • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    • AD6676 Why is the AD6676’s IF input resistance 60 ohms vs 50, 100 or even 200 ohms?
    • AD6676 Why isn't the noise floor of the AD6676 flat?
    • AD6676 I heard that Σ-Δ ADC’s can be driven into overload resulting in unstable behavior.  Is this true and should I be concerned?
    • Operating AD6676 at Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • +AD9560: FAQ
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?

I am familiar with typical ADC ac performance specifications such as SNR, SINAD, THD, SFDR, and ENOB when comparing ADC’s with each other. The AD6676 uses different specifications to quantify its ac performance characteristics. Why?

Since the AD6676 is a wideband IF receiver subsystem and utilizes a band-pass Σ-Δ ADC, other ac performance metrics that have more significance in the design of IF receiver are used.

For example, the “shaped” noise floor as described in AD6676 FAQ: Why isn't the noise floor of the AD6676 flat? occurs over a user-specified IF pass band that can be much less than the output bandwidth supported by the AD6676’s complex output data rate (FDATA_IQ). This makes SNR impractical since SNR for a typical ADC is defined over its entire Nyquist bandwidth (FADC/2).   The Noise Spectral Density (NSD) characteristics as well as its integrated in-band noise (IBN) performance (measured over a specified bandwidth and IF pass band region) provide more insight to a user on how the AD6676’s noise performance will affect their system performance in the demodulation of narrow band or wide band signal situated across the IF pass band. Since the AD6676 defines its full-scale level in dBm (PIN_0dBFS), an equivalent NF can be easily determined by the “spot noise” or NSD measured at a particular point in the pass band region.

Tags: wideband_if evaluation-system ad6676 high_speed_adc high_speed_ad_converter high_speed_converters if_sampling_adc wideband_if_receiver_subsystem high_speed_analog_to_digital_converter Show More
  • Share
  • History
  • More
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved