Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

     

    ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​

    By Ashish Iskande What is Tool Qualification and Why is it Important? In safety-critical automotive development, tools act as silent partners but can...

    Latest Blogs

    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
    • The ABCs of SerDes
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents What determines the AD6676’s full-scale input setting?
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • -AD6676: FAQ
    • I noticed that it is possible to further reduce the full-scale input power requirements to the AD6676.  Is there any trade-offs that I need to be aware of when considering this option?
    • Operating AD6676 at  Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
    • What determines the AD6676’s full-scale input setting?
    • What is the STF response of a Σ-Δ ADC and why does it matter?
    • AD6676 Can you explain what the “Profile feature” is and why I it may be advantageous to use in some applications?
    • AD6676 What development tools are available?
    • AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
    • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    • AD6676 Why is the AD6676’s IF input resistance 60 ohms vs 50, 100 or even 200 ohms?
    • AD6676 Why isn't the noise floor of the AD6676 flat?
    • AD6676 I heard that Σ-Δ ADC’s can be driven into overload resulting in unstable behavior.  Is this true and should I be concerned?
    • Operating AD6676 at Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • +AD9560: FAQ
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

What determines the AD6676’s full-scale input setting?

To a first order, the full-scale setting (PIN_0dBFS) is given by the following equation with IDACIFS being the full-scale current setting of the 1st stage feedback DAC and  RIN being the IF input resistance.

 

PIN_0dBFS = 10 × log10(1/2 × RIN × IDAC1FS2)

 

IDACIFS can be varied over a 4 to 1 mA range thus allowing PIN_0dBFS to be varied over a 12 dB range. At the max setting of 4 mA and an RIN of 60 ohms, the theoretical PIN_0dBFS is -3.2 dBm.  In practice, the IF, FADC, and Lext settings have a secondary affect that may result in the PIN_0dBFS being up to 1 dB higher than the theoretical value.

Tags: if_sampling ad6676 high_speed_adc high_speed_ad_converter sigma-delta if_sampling_adc vhf high_speed_analog_to_digital_converter Show More
  • Share
  • History
  • More
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved