Locale Icon
English
  • Forums

    Popular Forums

    • LTspice
    • RF and Microwave
    • Video
    • Power Management
    • Precision ADCs
    • FPGA Reference Designs
    • Linux Software Drivers

    Product Forums

    • Amplifiers
    • Microcontrollers
    • Clock and Timing
    • Data Converters
    • Direct Digital Synthesis (DDS)
    • Energy Monitoring and Metering
    • Interface and Isolation
    • MEMS Inertial Sensors
    • Power Management
    • Processors and DSP
    • Switches/Multiplexers
    • Temperature Sensors
    • Voltage References
    View All

    Application Forums

    • A2B
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
    • Design Tools and Calculators
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
    The Burning Question: How can ADI Solutions Ensure Rechargeable Device Batteries are Genuine?

    On the global stage, products and equipment using rechargeable batteries continue to proliferate exponentially, expecting to reach a staggering $170B market...
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
    • Maximize Your Power Regulator: Key Considerations for Thermal Performance
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quizzes AQQ294 about a digital phase splitter design

      1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Let's Take a Field-Bus Trip Your field-bus engines...
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
    Balancing Enhanced Radar Resolution with FPGA-Based Pulse Compression

    Radar and sonar systems must balance range resolution with the energy required for reliable detection. Pulse compression resolves this by sending a long...

     

    ​​ISO 26262 Essentials: Ensuring Confidence in Your Software Tools ​

    By Ashish Iskande What is Tool Qualification and Why is it Important? In safety-critical automotive development, tools act as silent partners but can...

    Latest Blogs

    • Step-by-Step: Implementing a Complete DSP Chain for Signal Analysis
    • Galvanic Isolation in SMPS: Ensuring Safety and Protection: Part 1 of 4
    • Mature, Not Old! The Longevity of 4 – 20 mA
    • Turning up the Noise: .NOISE Simulations in LTspice: Part 1 of 3
    • The ABCs of SerDes
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents What is the STF response of a Σ-Δ ADC and why does it matter?
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • -AD6676: FAQ
    • I noticed that it is possible to further reduce the full-scale input power requirements to the AD6676.  Is there any trade-offs that I need to be aware of when considering this option?
    • Operating AD6676 at  Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
    • What determines the AD6676’s full-scale input setting?
    • What is the STF response of a Σ-Δ ADC and why does it matter?
    • AD6676 Can you explain what the “Profile feature” is and why I it may be advantageous to use in some applications?
    • AD6676 What development tools are available?
    • AD6676 What is the difference between a typical IF-sampling ADC and the AD6676 and why is called a Wideband IF Receiver Subsystem?
    • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    • AD6676 Why is the AD6676’s IF input resistance 60 ohms vs 50, 100 or even 200 ohms?
    • AD6676 Why isn't the noise floor of the AD6676 flat?
    • AD6676 I heard that Σ-Δ ADC’s can be driven into overload resulting in unstable behavior.  Is this true and should I be concerned?
    • Operating AD6676 at Fadc of 3.26GHz or higher when max allowed specification is 3.2 GHz.
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • +AD9560: FAQ
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

What is the STF response of a Σ-Δ ADC and why does it matter?

The STF refers to the signal transfer function of the modulator or in practical terms, its input frequency response.  Traditional high-speed ADC’s based on a pipeline architecture typically have a low pass frequency response with the roll-off in response being attributed to its internal sample-and-hold (SHA) circuit or a buffer that may precede it. The AD6676 is based on a 6th order continuous-time band pass architecture displaying a wideband bandpass frequency response relative to its IF bandwidth setting (region of low noise spectral density). Large signals falling outside the IF passband region may not experience significant attenuation (before digital filtering).  As a result, one also should consider the impact of any large out-of-band signal on the AD6676’s performance when optimizing IF filtering and AGC operation.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • AD9083 : Analog input characteristics (STF)
    y_suzuki
    Hello, In "TERMINOLOGY" section of the datasheet, it is written as "STF is the frequency response of the ADC output signal relative to a swept single tone at the ADC input. The Typical Performance Characteristics...
  • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    stephenv
    I am familiar with typical ADC ac performance specifications such as SNR, SINAD, THD, SFDR, and ENOB when comparing ADC’s with each other. The AD6676 uses different specifications to quantify its ac performance...
  • RE: AD6676 70MHz bandwidth
    FormerMember
    Hello, I have contacted you by email so that I can set some STF plots that show sensitivity of frequency response when operating with low IF's and CLK rate. Regards..
 
Related Content
  • AD9083 : Analog input characteristics (STF)
    y_suzuki
    Hello, In "TERMINOLOGY" section of the datasheet, it is written as "STF is the frequency response of the ADC output signal relative to a swept single tone at the ADC input. The Typical Performance Characteristics...
  • AD6676 Why are the performance specifications of the AD6676 different than the ones used to specify a typical ADC?
    stephenv
    I am familiar with typical ADC ac performance specifications such as SNR, SINAD, THD, SFDR, and ENOB when comparing ADC’s with each other. The AD6676 uses different specifications to quantify its ac performance...
  • RE: AD6676 70MHz bandwidth
    FormerMember
    Hello, I have contacted you by email so that I can set some STF plots that show sensitivity of frequency response when operating with low IF's and CLK rate. Regards..
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
©2025 Analog Devices, Inc. All Rights Reserved
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
©2025 Analog Devices, Inc. All Rights Reserved