Join us for an exciting webinar where we will unveil and demonstrate our new bulk ordering and bulk quoting tools! Discover how you can streamline your...
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
      1. First, the quote of the week: " The best measure of a man's honesty isn't his income tax return. It's the zero adjust on his bathroom scale " - Unknown...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    How can we meet the growing power requirements of the future? 5G network deployments necessitate high-efficiency power conversion solutions capable of...

     

    Freedom from Interference: Control of Mixed ASIL Criticalities

    Interference, within the context of Functional Safety, refers to a situation in which a failure in a component of a system may propagate to other components...

    Latest Blogs

    • High-Tech Pro and Crafty Creator: Meet Iulia, Our Inspiring Super User!
    • Apples and Oranges: A Comparative Study of DCM and CCM: Part 6 of 6
    • Understanding AXI-Stream Interfaces for DSP Data Pipelines
    • Importing Op Amp Models in LTspice: When All Else Fails, Customize the Symbol: Part 3 of 3
    • Inside the Bits: Digging Deeper with Part-Specific Register Examples
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
High-Speed ADCs
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
High-Speed ADCs
  • Data Converters
High-Speed ADCs
Documents How to set the frequency of AD9560 PWM generator
  • Forums
  • File Uploads
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • HIGH-SPEED ADC SUPPORT COMMUNITY
  • TAGS LIST: High-Speed ADCs
  • +Absolute Group Delay: FAQ
  • +AD6620: FAQ
  • +AD6624A: FAQ
  • +AD6633: FAQ
  • +AD6635: FAQ
  • +AD6636: FAQ
  • AD6640: FAQ
  • +AD6640AST: FAQ
  • +AD6643: FAQ
  • +AD6644: FAQ
  • +AD6645: FAQ
  • +AD664: FAQ
  • +AD6650: FAQ
  • +AD6654: FAQ
  • +AD6655: FAQ
  • +AD6657: FAQ
  • +AD6676: FAQ
  • +AD9027: FAQ
  • +AD9042: FAQ
  • +AD9050: FAQ
  • +AD9054A: FAQ
  • +AD9057: FAQ
  • +AD9066: FAQ
  • +AD9200: FAQ
  • +AD9201: FAQ
  • +AD9211: FAQ
  • +AD9212: FAQ
  • +AD9215: FAQ
  • +AD9218: FAQ
  • +AD9220: FAQ
  • +AD9222: FAQ
  • +AD9224: FAQ
  • +AD9225: FAQ
  • +AD9228: FAQ
  • +AD9229: FAQ
  • +AD9230: FAQ
  • +AD9231: FAQ
  • +AD9233: FAQ
  • +AD9236: FAQ
  • +AD9238: FAQ
  • +AD9239: FAQ
  • +AD9240: FAQ
  • +AD9243: FAQ
  • +AD9244: FAQ
  • +AD9245: FAQ
  • +AD9246: FAQ
  • +AD9248: FAQ
  • +AD9249: FAQ
  • +AD9250: FAQ
  • +AD9253: FAQ
  • +AD9254: FAQ
  • +AD9255: FAQ
  • +AD9257: FAQ
  • +AD9261: FAQ
  • +AD9262: FAQ
  • +AD9265: FAQ
  • +AD9268: FAQ
  • +AD9266: FAQ
  • +AD9269: FAQ
  • +AD9271: FAQ
  • AD9272: FAQ
  • +AD9277: FAQ
  • +AD9279: FAQ
  • +AD9280: FAQ
  • +AD9283: FAQ
  • +AD9284: FAQ
  • +AD9286: FAQ
  • +AD9288: FAQ
  • AD922X: FAQ
  • +AD9410: FAQ
  • +AD9430: FAQ
  • +AD9432: FAQ
  • +AD9433: FAQ
  • +AD9434: FAQ
  • +AD9444: FAQ
  • +AD9446: FAQ
  • +AD9460: FAQ
  • +AD9461: FAQ
  • +AD9467: FAQ
  • +AD9481: FAQ
  • +AD9484: FAQ
  • AD9520: FAQ
  • -AD9560: FAQ
    • How to set the frequency of AD9560 PWM generator
  • +AD9600: FAQ
  • +AD9613: FAQ
  • +AD9625: FAQ
  • +AD9626: FAQ
  • +AD9627: FAQ
  • +AD9631: FAQ
  • +AD9640: FAQ
  • +AD9643: FAQ
  • +AD9644: FAQ
  • +AD9645: FAQ
  • +AD9649: FAQ
  • +AD9652: FAQ
  • +AD9680: FAQ
  • +AD9683: FAQ
  • +AD9684: FAQ
  • +AD9695: FAQ
  • +AD9814: FAQ
  • +AD9822: FAQ
  • +AD9826: FAQ
  • +AD9864: FAQ
  • +AD9874: FAQ
  • +AD96685: FAQ
  • +High Speed ADC: FAQ
  • +High Speed Capture Data: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +JESD204B: FAQ
  • +AD10200: FAQ
  • +AD10465: FAQ
  • +AD608: FAQ
  • +AD7720: FAQ
  • +AD8283: FAQ
  • +AD9211-300EBZ: FAQ
  • +AD9215BCPZ-105: FAQ
  • +AD9216: FAQ
  • +AD9257S: FAQ
  • +AD9629: FAQ
  • +AD9635: FAQ
  • +AD9637: FAQ
  • +HMCAD1520: FAQ
  • +MAX11835EWA+_B1: FAQ
  • +MAX11855: FAQ
  • +MAX1421ECM+: FAQ
  • +MAX1437BETK+_T1: FAQ
  • +MAX1448: FAQ
  • +MAX19515: FAQ
  • +MAX19516: FAQ
  • +MAX19516ETM+: FAQ
  • +MAX19517EVKIT+: FAQ

How to set the frequency of AD9560 PWM generator

Q 

I am working on the design of the analog interface of a SmartCard
reader/tester/ encoder.

I am currently evaluating the AD9560 pulse width modulator. This product, (or
its equivalent AD9561) would be perfect for our PWM needs, except for the Rset:
this resistor implies that operation has to be done at a single frequency.
However, in my application, I would like to change the frequency from 500kHz to
30MHz...

Is it possible to replace Rset with a DAC or a digital potentiometer, for
example...? Which voltage or current range should I use with a DAC? NB: It is
important that the precision on the duty cycle remains under 2%.

 

A 

Here are some ideas for setting the Rset resistance.

The purpose of Rset is to set the current, which charges an internal capacitor
to generate the internal voltage ramp. This ramp is the basis of the PWM
generator timing. Since the on-chip timing circuits vary from lot to lot and
can drift with temperature, an auto-calibration function adjusts the current
source so that the ramp duration is matched to the CLOCK input.

The attached diagrams show the simplified internal circuitry connected to the
Rset pin and a suggested way of connecting an external digital potentiometer.
The Rset node is sensitive to external capacitance, and since digital pots can
contribute significant parasitic capacitance, it is recommended that a fixed
resistor Ra be connected to pin 15, to isolate the device from external
capacitance. Choose Ra to be slightly less than Rset_min and choose Rb to be
slightly twice more than Rset max
requirement. Then, Rpot range should be 0 ohms to Rb's value.

The Rset only needs to set the current source to APPROXIMATELY the correct
value; the auto-calibration circuit will "fine-tune" the current source, so
that the datasheet specifications can be met. The guideline given in the
datasheet is that the nearest 1% resistor to the nominal value should be
chosen. So our "automatic" Rset should contribute an error no greater than the
nearest 1% resistor would. There are 96 standard values of 1% resistors in each
decade
(10k,10.2k,10.5k ... 97.6k,100k...) So it is normally possible to choose a
resistor whose nominal value is within 1% to 1.2% of the exact value you
require. This resistor may in turn have a value within +/-1% of it's nominal
value. So we end up with a worst case error band of +/-2.2% at room temperature.

For your stated frequency range, the resistor values are as follows
500kHz => 115.9kOhms
30MHz => 1.687kOhms

The problem with all "variable resistance" ICs (DACs, digital pots) is that the
ABSOLUTE value of the resistors is not so accurate (you must reckon with +/-20%
to +/-40%). What allows the very high precision is the RELATIVE MATCHING of the
on-chip resistors. In your application you need the absolute value of the
resistor to be within 2% to allow the autocalibration to operate.

1. Digital potentiometer. Easy to use. You can use three in series to give you
the variation in gain that you're looking for. The attached application note
shows the considerations when combining several digital pots.

2. Using the variable resistance from a Multiplying DAC. This offers higher
resolution and a wider choice of parts than the digital potentiometer solution.
However, you need to be careful to keep certain nodes at the same potential or
else the DAC behaves non-linearly. It may be harder to select a DAC with the
absolute rsistance value you require. I have attached a full reference from our
CMOS DAC Application guide. Suitable DACs would be any CMOS Iout, multiplying
DAC. e.g. AD7524, AD7533, AD7943, AD7945, AD7948.

Tags: ad9560
  • Share
  • History
  • More