AD9517 configuration through SPI Controller software

How to configure AD9517 in AD9268 Evaluation board using SPI Controller software? I am using HSC-ADC-EVALC board to connect AD9268 EVM

Parents
  • 0
    •  Analog Employees 
    on Jun 28, 2018 1:39 AM

    Hello,


    It is necessary to do some hardware modification and to follow the specific procedure to set up the AD9517 as the input clock to the AD9268 on the AD9268 Evaluation Board. I attach a file named "AD9268_9517_evb_setup.pdf" that show the steps to follow for setting up the AD9517 and AD9268 along with configuration file(.cfg) and cal file(.cal). I wish it works.

    Thanks

    Tony

    attachments.zip
  • Hi Tony,

    I'm also trying to evaluate AD9268 (S/N: 5602-017) using AD9517-4 clock synthesiser.

    I'm using HSC-ADC-EVALC board for configuring.

    I've followed the steps which you have mentioned, but the clock synthesizer is not locking (LED not turning RED). I've checked the SPI lines and there are signal transfer happening.

    I tried configuring the pin as Vs, but still no change. (The READ values are also not updating.

    Regards,

    Vishnu R.

Reply
  • Hi Tony,

    I'm also trying to evaluate AD9268 (S/N: 5602-017) using AD9517-4 clock synthesiser.

    I'm using HSC-ADC-EVALC board for configuring.

    I've followed the steps which you have mentioned, but the clock synthesizer is not locking (LED not turning RED). I've checked the SPI lines and there are signal transfer happening.

    I tried configuring the pin as Vs, but still no change. (The READ values are also not updating.

    Regards,

    Vishnu R.

Children
No Data