We use an external generator (CMOS output VCTCXO) to drive AD9864 CLK input.
We apply the signal as AC coupled as shown in the attached file.
Could you please inform me about driving necesities for CLK input of AD9864?
Abidin TASKIRAN
AD9864
Production
The AD9864 is a general-purpose IF subsystem that digitizes a
low level, 10 MHz to 300 MHz IF input with a signal bandwidth
ranging from 6.8 kHz to 270...
Datasheet
AD9864 on Analog.com
We use an external generator (CMOS output VCTCXO) to drive AD9864 CLK input.
We apply the signal as AC coupled as shown in the attached file.
Could you please inform me about driving necesities for CLK input of AD9864?
Abidin TASKIRAN
Hi Abidin,
Possibly to be assumed, but have you consulted the AD9864 datasheet? Lots of good information there.
http://www.analog.com/media/en/technical-documentation/data-sheets/AD9864.pdf
Best Regards,
Arik
Hi Arik,
Yes, i have consulted the AD9864 data sheet.
But, there isn't detailed information in it.
We designed our PCBs according to EVB schematic which shows AC coupled driving.
Thanks.
Abidin
Hi Arik,
Below message is received from Tony Ha and it clarifies the stuation.
***************************************************************************************************************************
****************************************************************************************************************************
Best regards,
Abidin
Hi Abidin,
So what specific concerns did you have with the clock input? In terms of driving and external clock (and Tony Ha had answer some of these questions), you would need to AC-couple the inputs unless 1.6V common-mode isn't and issue. 26MHz max.
The inputs are referenced to VDDC, so your input swing cannot be higher than this. The absolute max ratings for these pins tell you when damage to the part will occur.
You need to disable the internal LC tank circuitry to drive the clock externally.
Best Regards,
Arik
Hi Arik,
We solved the problem.
We recognized that It was related with ADC settings.
Thank you very much for you support.
Best regards,
Abidin