I have this HSC-ADC-EVALZ + AD9671EBZ development kit. I want to synchronise the capture with an external trigger, because I’m performing an FFT and I want the bins to correspond to the same part of the input sequence.
I found some FPGA files on this forum that should support sampling with an external trigger. Something like the example with the AD9656 ADC. In VisualAnalog, I’m using this bitstream: “ad9671_evalez_09292014_1025am.mcs”.
That’s why I asked if you could send me either a bitstream with functionality similar to the AD9656 project, or the original project with the missing cores, so that I can synthesise the bitstream with that functionality myself. I assume that ‘ad9671_evalez06132014_0921am.mcs’ contained this functionality. Also, if possible, could you send me the ISE 14.7 project for the combination with the AD9656?
Thank you.