Post Go back to editing

Common Mode Voltage & ADC input Voltage

Category: Hardware
Product Number: AD9257

Hello 

I am currently evaluating the AD9257-65 ADC for my application and would like your technical guidance regarding the analog input common-mode voltage, differential input swing, individual input voltage limits, digital output coding, and dynamic performance measurements.

According to the datasheet, the nominal input common-mode voltage (VCM) is approximately 0.9 V. However, on my hardware, I am measuring approximately 0.864 V at the ADC input common-mode node. Since this common-mode voltage will also affect my input-voltage and amplifier calculations, I would like to understand the acceptable tolerance and its impact on ADC performance and full-scale utilization.

I have the following questions:

1. ADC input common-mode voltage

The datasheet specifies an input common-mode voltage range. Could you please clarify whether the common-mode voltage of the AD9257-65 can be externally set within the specified range?

  • Is the ADC input common-mode voltage internally generated or does it need to be externally established?

  • What is the recommended method for setting the input common-mode voltage?

  • Can the VCM pin of the AD9257-65 be used to set the common-mode voltage of an external fully differential amplifier (FDA)?

  • Is there any recommended buffering or loading requirement for the VCM pin?

2. Measured VCM of 0.864 V

The nominal VCM is approximately 0.9 V, but I am measuring approximately 0.864 V in my hardware.

Could you please clarify:

  • Is 0.864 V an acceptable common-mode voltage for the AD9257-65?

  • What tolerance should I consider for VCM in my design calculations?

  • Should I use the nominal 0.9 V or the actual measured VCM when calculating the individual ADC input-voltage limits?

  • Can variation in VCM affect the achievable full-scale differential input range or ADC performance?

3. Full-scale 2 Vpp differential input

My fully differential amplifier is configured to provide a 2 Vpp differential output, corresponding to the specified differential input range of the AD9257-65.

Could you please clarify how the 2 Vpp differential input should be distributed between VIN+ and VIN−?

For example, if the common-mode voltage is 0.9 V and the differential input is 2 Vpp:

  • What should be the maximum and minimum voltage at VIN+?

  • What should be the maximum and minimum voltage at VIN−?

  • What is the recommended individual input-voltage swing for each ADC input?

  • Is the 2 Vpp specification defined as the voltage difference between VIN+ and VIN−, or is there any other consideration when determining the individual input swings?

4. Individual ADC input voltage versus differential input voltage

I would also like clarification regarding the relationship between the differential input specification and the absolute maximum rating of each ADC input.

For example, suppose my FDA produces:

VIN+ = −0.4 V
VIN− = +0.6 V

The differential voltage would be:

VIN+ − VIN− = −1.0 V

However, VIN+ would be below the specified absolute maximum input voltage of −0.3 V.

In this situation:

  • Would the ADC be damaged?

  • Does this condition violate the ADC operating conditions?

  • Is the differential input voltage alone sufficient to determine whether the ADC input is within its valid operating range?

  • What individual VIN+ and VIN− limits should be considered during normal operation?

  • What is the digital code for this case that comes out from ADC

5. Example with 2 V differential input

Similarly, if the FDA produces:

VIN+ = −0.6 V
VIN− = +1.4 V

the differential voltage is:

VIN+ − VIN− = −2.0 V

However, VIN+ is below the −0.3 V absolute maximum rating.

Could you please clarify whether this condition can cause damage to the ADC, even though the differential voltage magnitude is 2 V?

More generally, should the individual ADC inputs always remain within a specific recommended operating range independent of the differential voltage?

6. How should the FDA output be configured to protect the ADC?

Since I am using a fully differential amplifier to drive the AD9257-65, I would like to understand how I should configure the FDA output common-mode voltage and differential swing so that:

  • The ADC achieves its maximum practical dynamic range.

  • Neither ADC input violates its recommended operating range.

  • Neither ADC input approaches or exceeds the absolute maximum rating.

  • The full 2 Vpp differential input range can be utilized.

Could you please provide the recommended relationship between FDA VOCM, VIN+, VIN−, and differential input voltage for this application?

7. DC input voltage to both ADC inputs

I would also like to understand how the ADC behaves when a DC voltage is applied to both differential inputs.

For example:

VIN+ = 0.9 V
VIN− = 0.9 V

or:

VIN+ = 0.864 V
VIN− = 0.864 V

In these conditions, the differential input is 0 V.

Could you please clarify:

  • What DC input voltage range can safely be applied simultaneously to VIN+ and VIN−?

  • What common-mode voltage range should be maintained for normal operation?

  • How should I determine the valid DC voltage range for each individual input?

  • Is there a recommended DC input condition that corresponds to ADC midscale?

8. Offset Binary and Two's Complement output format

I would also appreciate clarification regarding the AD9257-65 digital output coding.

The ADC is a 14-bit ADC, and I understand that it supports both Offset Binary and Two's Complement output formats.

Could you please explain:

  • Which output format is selected by default?

  • How is the digital output code related to the differential analog input voltage?

  • What digital code should I expect at zero differential input?

  • What digital code should I expect at +0.5 V differential input?

  • What digital code should I expect at −0.5 V differential input?

  • What digital code should I expect at the positive and negative full-scale differential inputs?

For example, if the differential input voltage is:

VIN+ − VIN− = +1.0 V

could you please provide the expected 14-bit digital output code for both:

  1. Two's Complement

  2. Offset Binary

I would also like to confirm whether the following approach is correct for calculating the ADC LSB and digital counts:

ADC resolution = 14 bits

Number of codes = 2^14

Differential full-scale range = 2 Vpp

Should the ADC digital count be calculated using:

{V_diff}/{2V{peak to peak}*(2^{14}-1)

or is another transfer-function equation recommended for the AD9257-65?

For Offset Binary, is adding 8192 to the signed two's-complement representation the correct way to convert between the two coding formats, or is there a specific ADC transfer-function convention that should be followed?

9. Measuring actual ADC digital counts

Could you please recommend a procedure for experimentally verifying the ADC transfer function?

I would like to apply known differential DC voltages to the ADC input and record the corresponding FPGA output codes.

For example, I would like to test:

0 V differential
+0.25 V differential
+0.5 V differential
+0.75 V differential
+1.0 V differential

and

−0.25 V differential
−0.5 V differential
−0.75 V differential
−1.0 V differential

What test setup and calculation method would you recommend for comparing the measured FPGA  ADC codes with the expected theoretical codes?

10. SNR, SINAD, ENOB and SFDR measurement

Finally, I would like to measure the actual ADC performance on my hardware.

Could you please recommend the appropriate procedure for measuring:

  • SNR

  • SINAD

  • ENOB

  • SFDR

  • Noise floor

using the AD9257-65 and an FPGA-based data-capture system?

In particular:

  • What input signal amplitude should be used?

  • What input frequency is recommended?

  • What sampling frequency should be used?

  • How many ADC samples should be captured?

  • Should coherent sampling be used?

  • What FFT size is recommended?

  • Which FFT bins should be included when calculating noise power?

  • How should the fundamental and harmonics be treated when calculating SNR, SINAD, and SFDR?

  • How should ENOB be calculated from the measured results?

I would like to compare my measured results with the performance specified in the AD9257-65 datasheet.

11. Overall design clarification

My objective is to correctly configure the fully differential amplifier → AD9257-65 interface so that I can utilize the ADC's available dynamic range while maintaining the appropriate common-mode voltage and individual input-voltage limits.

Could you please provide a recommended set of equations or an example showing the relationship between:

FDA VOCM → VIN+ / VIN− → differential input voltage → ADC digital code

including the appropriate treatment of Offset Binary and Two's Complement?

Since the measured common-mode voltage in my hardware is approximately 0.864 V instead of the nominal 0.9 V, clarification on this point is particularly important because it will directly affect my amplifier output-voltage calculations and ADC input-range calculations.

Thank you for your support.

Best regards,
Nishant Gupta

Parents
  • Hi  

    1. The analog inputs of the AD9257 are not internally dc-biased. An external circuit establishes the common-mode voltage at VIN+ and VIN-. The device provides an internally generated common-mode reference at the VCM pin, which may be used to bias the input network or supply it to the VOCM pin of a compatible FDA. For optimum performance, the datasheet recommends:

    The device can operate over a wider common-mode range, as shown in Figure 44, but 0.9 V is the recommended operating point. (Note: You cannot program the output of the VCM pin of the AD9257)

    The AD9257 VCM pin can be used to set the common-mode voltage of an FDA. Provided that the FDAs input common-mode range is within the VCM pin output voltage (VCM = 0.9V). (Note: VCM pin has maximum current load of about 1mA to 1.5mA)

    2. A measured VCM of 0.864 is reasonably close to the recommended 0.9V common-mode voltage. Figure 44 shows the ADC functioning over a wider common-mode range. The data sheet does not specify VCM-output tolerance but rather an operating point. For calculations, use the actual measured common mode to determine the instantaneous measured pin voltages.

    3.For a 2 V p-p analog input:

    For a balanced differential signal:

    A 2 V p-p differential signal has:

    Therefore, each individual line has:

    With Vcm = 0.9V:

    Thus, both inputs swing between 0.4V and 1.4V:

    Differential Output: 

    4. The voltage on VIN+ and VIN− should remain within −0.3 V to 2.0 V, as specified by the datasheet absolute maximum ratings. Exceeding these limits may result in degraded operation or potential damage to the ADC. The 2 V p-p differential input range is defined by the ADC reference voltage (VREF = 1 V). The reference voltage sets the ADC's full-scale differential input range; therefore, both the individual input voltages and the differential input voltage must remain within their respective limits.

    If your FDA produces VIN+ = -0.4 V and VIN− = +0.6 V, the differential voltage is -1.0 V, which is within the ADC's full-scale differential range. However, VIN+ exceeds the absolute maximum rating because it is below -0.3 V. Therefore, this condition is outside the valid operating range of the ADC and could potentially damage the ADC if it is sustained for extended periods.

    To ensure proper operation, each input pin (VIN+ and VIN−) should remain within the specified input voltage range of -0.3 V to 2.0 V. In addition, the differential input voltage should remain within the ADC's full-scale input range of 2 V p-p when VREF = 1 V.

    5. For the stated instantaneous voltages: Vin + = -0.6V and Vin - = 1.4V

    This is not a valid negative full-scale condition for a 2 V p-p differential ADC range. The valid differential range is -1V to 1V (2Vpp).

    A differential value of −2.0 V is beyond negative full scale and will produce an overrange or clipped output code. In addition, VIN+ = −0.6 V violates the −0.3 V absolute maximum rating.

    In addition, VIN+ = -0.6 V exceeds the absolute maximum rating of the VIN+ pin. This condition may cause the waveform to be clipped and could potentially degrade the performance of the ADC if sustained for an extended period of time. To ensure proper operation, both VIN+ and VIN− should remain within the specified input voltage range of -0.3 V to 2.0 V. Operating either input outside this range may result in clipping and could potentially degrade the performance of the ADC.

    6.Configure the FDA output common-mode voltage to approximately 0.9 V, preferably using the AD9257 VCM output if it is compatible with the FDA VOCM input and does not excessively load the VCM pin. Decouple the ADC VCM pin to ground with 0.1 µF.

    For a full-scale 2 V p-p differential signal, configure each FDA output to swing 1 V p-p, or ±0.5 V peak, around 0.9 V. VIN+ and VIN− must be equal in amplitude and 180° out of phase. Each ADC input therefore swings from approximately 0.4 V to 1.4 V

    7. The input voltage applied should be within the absolute maximum ratings of the device and should not be operated at or beyond its recommended value. The datasheet recommends VCM = 0.9V for optimal performance.

    8. By default, the AD9257 digital output is set in two’s complement this can be set by configuring the appropriate register. You may refer to this app note for further discussion about digital outputs: MT-009: Data Converter Codes-Can You Decode Them?

    10. For detailed discussion for measuring the actual ADC performance you may refer to these application notes:

    1. AN-835: Understanding High Speed ADC Testing and Evaluation | Analog Devices,
    2. MT-003:Understand SINAD, ENOB, SNR, THD, THD + N, and SFDR so You Don't Get Lost in the Noise Floor
    3. Defining and Testing Dynamic Parameters in High-Speed ADCs, Part 1 | Analog Devices
    4. Dynamic Testing of High-Speed ADCs, Part 2 | Analog Devices
    5. MT-010: The Importance of Data Converter Static Specifications-Don't Lose Sight of the Basics! 

    11. You may refer to my answer in bullet number 3 for VIN and VCM.

    I attached some reference app notes that might be useful to you:

    MT-075: Differential Drivers for High Speed ADCs Overview (analog.com)
    AN-1026: High Speed Differential ADC Driver Design Considerations | Analog Devices
    AN-0990: Terminating a Differential Amplifier in Single-Ended Input Applications | Analog Devices
    AN-2539: Single-Supply, DC-Coupled 16-Bit, 125 MSPS Analog Front End for Bipolar Input Signals | Analog Devices

    • Hello,

      Could you please provide the internal architecture details of this pipeline ADC, particularly the relevant internal capacitance values and sampling/hold capacitor information?

      I am currently designing the input filter and would like to accurately determine the required C_SH (sample-and-hold capacitance), acquisition time, and appropriate filter cutoff frequency for stable and optimized ADC operation.

      If available, could you please provide the following information:

      1. Internal sample-and-hold/sampling capacitor (C_SH) value or its equivalent input capacitance.
      2. Any relevant internal switching capacitance or capacitor network associated with the ADC input.
      3. Acquisition time and settling requirements of the input sampling network.
      4. Recommended source impedance and input RC filter configuration for the ADC.
      5. If available, an SPICE model or behavioral model that includes the relevant input sampling characteristics and internal capacitances.

      The objective is to model the ADC input network in SPICE and determine the appropriate RC filter values and cutoff frequency while ensuring adequate settling and smooth operation at my intended sampling and input signal frequencies.

       an equivalent input model or recommended simulation model that represents the ADC's sampling behavior would also be very helpful.

      Thank you 

    • How can I best utilize VisualAnalog for my custom ADC design, considering that there is no corresponding evaluation board available? Please suggest what parameters or aspects of the ADC signal chain I can simulate in VisualAnalog and what useful analysis/results I can extract from it for optimizing and validating my design.

    • Hi  

      The AD9257 uses a unbuffered input architecture, as such, to model its analog input you should use its S-parameter model that can be found in the product page. For reference: A Resonant Approach to Interfacing Amplifiers to Switched-Capacitor ADCs Application Note (AN-827)

    • Hi  

      You may use VisualAnalog to estimate the expected ADC performance under different operating conditions. For example, you can evaluate the effects of clock jitter on performance of the ADC and observe the expected output in both time and frequency domains for a given input signal. This allows you to analyze metrics such as SNR, SFDR, SINAD, Harmonic distortions, and noise floor to help optimize and validate your design. 

      See App Note for detailed discussion: AN-905: VisualAnalogTm Converter Evaluation Tool Version 1.0 User Manual | Analog Devices

    Reply Children
    No Data

    Before You Switch


    Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.