Hi
We have build a test board with four AD9645/55 ADC featuring a 8 channel ADC system with 125Ms/s.
The system can be equipped with the AD9645(14bit) AD9655(16bit) ADC. Both show a much larger DC cross talk than specified in the datasheet.
We measure between two channels on the same chip a DC cross talk of around 0.05-0.2% (~60db).
We tested it with on board DACs as well as with external pulse generators (20usec length) by pulsing on channel and measure the response on the other not connected one.
We have also disabled the ADA4930 front end buffer and supplied the signals from pulse generator to the ADC chip directly (including the correct OCM voltage). But this has no effect too.
Larger blocking of Vref has no effect.
The cross talk is independent of the offset (10000-50000LSB) of the signals and have slight dependency from the OCM supplied to the ADC (0.5-1.2V).
The only strong dependency is seen is by changing the temperature. Some channels get worse with higher temperature some become better. Some are excellent at exactly one specific temperature.
Even making a short cut to Vocm (suplied internal or external) to the both inputs of the unconnected channel makes no difference.
On the other channels on the board not on the same chip have no visible/measurable cross talk. Power supply is very stable and no effect can be be seen during the injected pulses!
The manual (ad9645) says that cross talk should be -97db (or <0.001%)

but with the footnote
![]()
I do not really know how to measure cross talk at 70Mhz with a 125MHz ADC and i have no idea what it means for the DC cross talk !?!
Is there any DC cross talk measurement for the above chips?
Or do you have any idea what might wrong with our setup ?
Thanks
Thomas