Post Go back to editing

ad9645 internal/external Vref

Thread Summary

The user questioned the AD9645's VREF pin functionality, noting the datasheet's contradiction between marking it as output only and specifying an input resistance. The final answer clarified that the AD9645's VREF is an output-only pin with an internal 7.5 kΩ resistance, unlike the AD9655, which supports VREF as both input and output. The user's attempt to supply an external 1.2V reference via a 500Ω resistor did not affect the internal VREF, which remained at 1.0V. Feedback on the datasheet's clarity was appreciated and will be considered for future revisions.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9645

we are using the ad9645 and the manual is very unclear! 

in the pin description you find 

    

Vref is marked as output only 

in the DC specification you find 

the Voltage Reference has an input resistance!!!! 

Outputs have no input resistance! 

I assume there is something wrong! 

Has the ad9645 an input/output Vref or an output only??? 

Would be nice to make the manual more clear! 

Thanks  

Thomas 

Edit Notes

i forgot the ad9645 product in the subject
[edited by: mizzi at 1:05 PM (GMT -4) on 25 Jul 2026]
  • Hi  

    Thank you for using AD9645. We are looking into your query and will get back to you as soon as possible. 

  • Hi  

    The AD9645 generates VREF internally using an internal voltage reference circuit. As shown in Figure 52, the VREF pin includes an internal 7.5 kΩ resistance; therefore, the specified input resistance can be interpreted as the internal load connected to the VREF pin. Since the reference voltage is generated internally, the VREF pin can be treated as an output.

  • Hi  

    Just to add to my colleague's response, the AD9645 generates the reference voltage internally using an on-chip reference circuit. As shown in Figure 52 of the datasheet, the VREF pin includes an internal 7.5 kΩ resistance. Therefore, the "input resistance" specification should be interpreted as the internal resistance associated with the VREF node rather than indicating that the pin is intended to be driven by an external source.

    Since the reference voltage is generated internally, VREF should generally be treated as an output pin. We agree that the combination of an "output" pin description and an "input resistance" specification can be confusing, and we appreciate the feedback regarding the datasheet wording. We will take this feedback into consideration and work to clarify the VREF description in a future datasheet revision to help avoid similar confusion.

  • Hi JEstrella, , 

    thank for you answer! But ... 

    if you look to the AD9655 manual  (a pin compatible Chip with 16bit) you see exact the same Vref equivalent circuit. 

    the AD9655 has an Input/Output Vref pin which can be used as Input for the ADC reference.

    Are you sure that the AD9645 Vref is an output only?

    Or is it perhaps a Vref In/Out with overwrite from outside (as seen in many other ADCs). 

     

  • Hi  

    In the AD9655 datasheet, it is explicitly stated that the reference voltage (VREF) can be provided either internally or externally through register configuration. As such, the VREF pin on this device can function as either an input or an output.

    On the other hand, the AD9645 does not support this feature. Instead, the VREF pin is used only as an output from the device and cannot be driven by an external reference.

  • It was from my side a simple assumption because the data sheet was unclear and specifies a input resistance and also an absolute maximum rating. 

    Nevertheless we have supplied a slightly higher 1.2 V to the reference pin via a 500 ohm resistor but the gain has not changed and the Vref was still at 1.0V. 

    Would be nice if you correct the data sheet (the datasheet of ad9635 is the same way unclear).   

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.