Post Go back to editing

AD9689 JESD PLL Lock Issue at 1 GSPS

Category: Software
Product Number: AD9689
Software Version: RTL

Hi Team,

I am bringing up the AD9689 in Full Bandwidth Mode using RTL code based on the initialization sequence described in the AD9689 datasheet (Page 81).

The hardware being used is:

  • AD9689-2600EBZ Evaluation Board
  • ADS8-V1EBZ FPGA Carrier Board

At this stage, I am only checking the JESD PLL lock status and have not connected the JESD lanes to the FPGA yet.

Clock Input

A signal generator is connected to the AD9689 CLK+/- inputs.

Configuration Used:

The initialization sequence follows the datasheet example, with the following modifications for 1 GSPS operation:

  1. Register 0x056E = 0x10
    • JESD PLL lane-rate range selection
  2. Register 0x0590 = 0x0F
    • Subclass 0 operation

All other register writes and the initialization sequence are the same as the datasheet example.

After writing 0x14 to Register 0x0571 (JESD204B Link Power-Up), I wait 5 ms before reading the PLL status register (0x056F).

Issue Observed:

When the ADC sampling clock is 1 GHz, the readback from Register 0x056F is:

0x056F = 0x00

which appears to indicate that the JESD PLL is not locked.

However, when I configure the same hardware using the ACE software, the JESD PLL reports a locked condition.

For verification , I varied the ADC sampling clock frequency and re-ran the complete RTL initialization sequence each time and the readback details for the PLL lock are as follows:

Clock Register 0x056F
1.2900 GHz 0x80
1.2840 GHz 0x80
1.2835 GHz 0x88
1.2831 GHz 0x08
1.2825 GHz 0x08
1.2820 GHz 0x08
1.0000 GHz 0x00

I exported the ACE register configuration and compared it against my RTL configuration. The key JESD-related registers appear to match, but the ACE export contains approximately 577 register writes in total.

My questions are:

  1. Is the Page 81 initialization sequence sufficient for Full Bandwidth Mode at 1 GSPS, or are additional registers required beyond the documented sequence?
  2. Is Register 0x056E = 0x10 the correct setting for a 1 GSPS configuration with:
    • L = 8
    • M = 2
    • F = 1
    • Subclass 0
  3. Does the ACE software perform additional initialization steps that are required for reliable JESD PLL lock?
  4. If the full ACE-generated register set must be applied, is there a recommended register programming sequence that should be followed?

Any guidance on  the minimum required initialization sequence for 1 GSPS operation would be appreciated.

Thank you.

Parents
  • Hi  

    The AD9689-2600 is recommended to operate with a sampling clock from 1.9 GSPS to 2.7 GSPS, and operation outside this range is not recommended as ADC performance may degrade. While the device may appear functional at lower rates (e.g., 1 GSPS), this is outside the characterized operating region, so JESD PLL lock and overall performance are not guaranteed.
    Additionally, based on Figures 59 and 60 in the datasheet, the device is only characterized over approximately 1.8 GSPS to 2.7 GSPS, and the initialization sequence is intended for use within this range.

Reply
  • Hi  

    The AD9689-2600 is recommended to operate with a sampling clock from 1.9 GSPS to 2.7 GSPS, and operation outside this range is not recommended as ADC performance may degrade. While the device may appear functional at lower rates (e.g., 1 GSPS), this is outside the characterized operating region, so JESD PLL lock and overall performance are not guaranteed.
    Additionally, based on Figures 59 and 60 in the datasheet, the device is only characterized over approximately 1.8 GSPS to 2.7 GSPS, and the initialization sequence is intended for use within this range.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.