Post Go back to editing

Confirmation Request for AD9517 PECL Clock Path Rework on AD9434-FMC-500EBZ

Thread Summary

The user seeks confirmation for configuring the AD9517 PECL clock output path on the AD9434-FMC-500EBZ evaluation board to drive the AD9434 CLK+ / CLK- inputs with a 250 MHz clock. The final answer confirms the required modifications: install R208 (200 ohm), C302, C303, C304, C305, R307, R308, and C311; remove C209 and C210. Capacitor pads 6-9 and 7-10 correspond to C209 and C210, respectively, and should be removed. C304 uses pads 5-6, and C305 uses pads 7-8. Pads 1-2 and 3-4 are for C306 and C307, which should remain unpopulated, along with R311. No additional components need to be modified for this configuration.
AI Generated Content
Category: Hardware

I am submitting a corrected follow-up regarding my AD9434-FMC-500EBZ clock-path question. My previous comment referred to the AD9517 LVDS clock output path, but that was based on an incorrect interpretation of the schematic and should be disregarded.

I would now like to request confirmation specifically for the AD9517 PECL clock output path.

 

I am using an AD9434-FMC-500EBZ evaluation board, and I would like to use the onboard AD9517 clock path instead of the default direct clock path.

My goal is to use the onboard Y1 500 MHz oscillator as the AD9517 clock input, configure the AD9517 in distribution mode with a divide-by-2 setting, and drive the AD9434 CLK+ / CLK− inputs with a 250 MHz clock using the AD9517 PECL output path.

According to the schematic, my current understanding of the intended PECL clock path is:

Y1 500 MHz oscillator
→ R209 / T200 / OPT_CLK_P and OPT_CLK_N
→ C302 and C303 into the AD9517 CLK / CLK_N inputs
→ AD9517 divide-by-2 distribution mode
→ AD9517 OUT3 / OUT3_N PECL outputs
→ C304 and C305
→ AD9434 CLK+ / CLK− inputs

Based on this, I believe the required rework is:

* Install C302 and C303 = 0.1 uF
* Install C304 and C305 = 0.1 uF
* Install R208 = 200 ohm
* Remove C209 and C210
* Keep C300 and C301 unpopulated, because REFIN/REFIN_N are not used
* Keep C306 and C307 unpopulated, because the LVDS output path is not used
* Keep R311 unpopulated
* Keep R210 and R213 populated
* Keep R307 and R308 populated

I attached a photo of the actual PCB area near R208, C302, C303, C304, C305, C306, C307, C209, and C210.



For clarity, I numbered the 10 exposed capacitor pads in upper parts of the photo as follows:

1 2 3 4
5 6 7 8
  9 10

At the moment, the two populated capacitors appear to be connected as:

* 6 to 9
* 7 to 10

I believe these two populated parts are C209 and C210.

Could you please confirm the following?

1. Are the currently populated capacitors between pads 6–9 and 7–10 indeed C209 and C210?

2. For the AD9517 PECL clock path, should I remove the two capacitors currently installed at 6–9 and 7–10?

3. For C304 and C305, which pad pairs should be connected with 0.1 uF capacitors using the numbering above? My current understanding is:

* C304 = pads 5–6
* C305 = pads 7–8
Please confirm whether this is correct.

4. Are pads 1–2 and 3–4 for C306 and C307, and therefore not used for the PECL option?

5. For the AD9517 input clock path, C302 and C303 should also be populated with 0.1 uF capacitors to couple OPT_CLK_P / OPT_CLK_N into the AD9517 CLK / CLK_N inputs. Could you please confirm the physical pad locations of C302 and C303 in the attached photo, or indicate if they are outside the marked pad group?

6. Is R208 the resistor footprint directly above these capacitor pads in the photo, and should it be populated with 200 ohm for this AD9517 PECL clock option?

7. Should R311 remain unpopulated for the PECL option?

8. Are there any additional components that must be removed or populated for this AD9517 PECL clock configuration?

I want to avoid damaging the board by soldering the 0.1 uF capacitors to the wrong pads, so I would appreciate confirmation using the pad numbering above.

Thank you.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.