I would like to use the on-board Y1 oscillator as the ADC sample clock instead of an external clock source. However, in the schematic I noticed that R209 is marked as DNI.
Could you please confirm the following?
-
Can I use the on-board Y1 oscillator by populating R209 and setting the related jumper(s) appropriately?
-
If so, what exact rework or jumper configuration is required to enable Y1?
-
Does the Y1 path feed the ADC clock directly, or can it be routed through the AD9517 optional clock path?
-
If the AD9517 path can be used, is it possible to derive a clock rate that is more suitable for the ZedBoard reference design than the on-board 500 MHz oscillator frequency?
-
Is there an official or recommended clock configuration for using the AD9434-FMC-500EBZ with ZedBoard?
-
I have seen different schematic/document versions regarding the clock path. Could you please let me know which document or board revision I should follow for this configuration?
My main goal is to understand whether the on-board oscillator can be used reliably with ZedBoard, and if so, what the correct hardware configuration is.