Post Go back to editing

Request for Technical Support

Thread Summary

The user inquired about using the AD9650 ADC for video digitization. The AD9650, a dual 16-bit ADC with a 500 MHz analog input bandwidth and up to 105 MSPS, is suitable for video applications if the signal bandwidth and sampling requirements are within its limits. ADI also offers dedicated 10-bit Video ADCs, which are typically sufficient for video applications.
AI Generated Content
Category: Hardware
Product Number: AD9650

We need to confirm that this ADC AD9650 can be used in video digitization application.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.