The AD6641 datasheet specifies the Input Common-Mode Voltage of the Analog Inputs to be +1.8V TYP. It does not specify a range. How is the AD6641 able to operate at +1.8Vicm and 1.6Vpp (differential) when the chip is powered from a +1.9V supply? At 1.6Vpp (differential) each analog input would swing +/-400mV (800mVpp Single-Ended) around +1.8Vicm. That makes the peak analog input voltage +2.2V but the ABSOLUTE MAXIMUM RATING of VIN± to AGND is AVDD + 0.2V = +2.1V
Wouldn't it make more sense to operate at a lower input common mode voltage?