Hey
The LTC2239's mode-pin has 4 thresholds (0, 1/3Vdd, 2/3Vdd, Vdd).
Please advise me the tolerance of these thresholds.


regards.
Inon
LTC2239
Production
The LTC2239 is a 10-bit 80Msps, low power 3V A/D converter designed for digitizing high frequency, wide dynamic range signals. The LTC2239 is perfect for...
Datasheet
LTC2239 on Analog.com
Hey
The LTC2239's mode-pin has 4 thresholds (0, 1/3Vdd, 2/3Vdd, Vdd).
Please advise me the tolerance of these thresholds.


regards.
Inon
Hello INON, All assigned engineers are out of office currently. JAlipio will be back in the week of 1/7/2026 to answer your question!
Hi INON
Thanks for your interest in LTC2239.
The datasheet does not explicitly state the tolerance for these thresholds. However, mode-pin thresholds are typically designed to fall within a certain percentage of VDD, often around ±10%. To ensure reliable operation, it’s best to validate on hardware by slowly sweeping the mode voltage and observing the transition points with an oscilloscope.
Thanks for the clarification.
I’m trying to make sure the mode selection is solid across temperature, supply variation, and production spread. Since the datasheet doesn’t give min/max thresholds, do you have any characterized data, typical curves, or internal limits for the MODE pin comparators? Even a rough typical range would help with margining.
If there’s no characterization data available, can you confirm that the ±10% guideline is what you recommend designing around?
Thanks,
Inon
Hello,
The thresholds used by comparators that compare the MODE voltage are likely set to 0.25 VDD, 0.5 VDD, and 0.75 VDD. These voltages will be accurate to better than 0.1% since they are based on a resistor ladder consisting of 4 equal resistors with the 3 taps generating the ratio metric values above.
As a result.......using standard 1% resistors to generate 0.33 VDD and 0.67 VDD (via a two resistor ladder) should provide sufficient accuracy to stay clear of these thresholds.