Suppose i need to read the parellel bits from the adc and send it to a software for displaying. What domain of microcontrollers should i choose? I have STM Nucleo-H753ZI, which uses STM32H753ZI MCU, is it an apt choice?
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
AD9215
Production
The AD9215 is a family of monolithic, single 3 V supply, 10-bit, 65/80/105 MSPS analog-to-digital converters (ADC). This family features a high performance...
Datasheet
AD9215 on Analog.com
Suppose i need to read the parellel bits from the adc and send it to a software for displaying. What domain of microcontrollers should i choose? I have STM Nucleo-H753ZI, which uses STM32H753ZI MCU, is it an apt choice?
Hello kraken618, All assigned engineers are out of office currently. JAlipio will be back in the week of 1/7/2026 to answer your question!
Hi kraken618
Thanks for your interest in AD9215.
AD9215 outputs parallel CMOS data at up to 105 MSPS. That means 105 million samples/sec × 10 bits ≈ 1050 Mbps raw data.
For this data rate, an FPGA or an ADC evaluation board with integrated FPGA such as HSC-ADC-EVALCZ which is based on Virtex-4 is recommended. A microcontroller or STM32 board cannot reliably handle the throughput without significant decimation, potential data loss, and additional external logic or FIFO buffering.
OK Thanks