I am using the HSC-ADC-EVALCZ board (Virtex-4 FPGA) to evaluate the AD9253 ADC (AD9253_125EBZ). If possible, could you please share the default FPGA design and UCF/constraint files from which the FPGA binary (.bin) file is generated, which is then used by VisualAnalog, for the HSC-ADC-EVALCZ with the AD9253-125EBZ?
Access to the original constraints would help me better understand how the LVDS inputs are configured, particularly since Virtex-4 does not support the LVDS_18 IOSTANDARD. Specifically, it would clarify whether the reference design keeps the FPGA I/O bank at 1.8 V while using LVDS_25, or whether the FPGA bank voltage should be changed to 2.5 V using jumper J9 on HSC-ADC-EVALCZ board. It would also help me understand the deserialization format and data alignment logic used in the reference design, enabling me to base my custom FPGA implementation on the same proven and validated configuration.