ADA4945-1
Recommended for New Designs
The ADA4945-1 is a low-noise, low-distortion, fully differential amplifier with two selectable power modes. The device operates over a broad power supply...
Datasheet
ADA4945-1 on Analog.com
AD9467
Recommended for New Designs
The AD9467 is a 16-bit, monolithic, IF sampling analog-to-digital converter (ADC). It is optimized for high performance over wide bandwidths and ease of...
Datasheet
AD9467 on Analog.com
Hello Analog Devices Team,
I am working with the AD9467 (16-bit, 250 MSPS) ADC and using ADA4945-1 (full-power mode) as the front-end differential driver. My goal is to capture low-frequency digital signals such as:
PWM signals from Arduino / Raspberry Pi (kHz to a few MHz)
CAN bus physical-layer waveforms
Source: Arduino / Raspberry Pi PWM or CAN signal (single-ended)
Conditioning: ADA4945-1 configured as single-ended to differential
ADC: AD9467 FMC board
ADC input connected via SMA (J100)
To support DC-coupled operation, I modified the AD9467 FMC front end:
Removed input transformers and AC-coupling capacitors
Initially removed R111 / R112 / C107 (ADC VCM bias network)
Later re-installed R111 / R112 / C107
Tested multiple configurations:
OUT+ only (single-ended into ADC)
OUT+ → VIN+, OUT− → VIN− (true differential)
At higher-frequency sine waves (tens of MHz), the ADC behaves as expected
For low-frequency PWM / square signals, the ADC output becomes:
Flat line
Or shows sporadic spikes / unstable levels
ADA4945 outputs look correct on an external oscilloscope
Output common-mode is ~2.15 V, matching AD9467 requirements
Is it architecturally valid to use:
ADA4945-1
to extract low-frequency PWM / digital signals (kHz–MHz range) from microcontrollers and CAN bus sources when driving the AD9467?
Or is the AD9467 + high-speed differential driver not suitable for reliable capture of:
DC-coupled
Low-frequency
Large duty-cycle digital waveforms?
Specifically:
Is the flat ADC output expected behavior due to sampling capacitor charge settling at low frequencies?
Is a different ADC architecture (e.g., SAR ADC) recommended for such signals?
Is there a recommended front-end topology for mixed-signal (PWM + CAN + analog) capture using AD9467?
Any guidance on whether this use case is supported, discouraged, or requires additional circuitry would be greatly appreciated.
Thank you for your time and support.
Best regards,
Sai Teja
Hi Saitej
Thank you for using AD9467.
This is to acknowledge your query, kindly give us some time to get back to you.