Post Go back to editing

AD9467-FMC-250EBZ – Is DC-Coupled Single-Ended Drive Using VCM Bias Electrically Valid After Removing Transformer Stage?

Thread Summary

The user asks if the AD9467 ADC can be operated in a single-ended + VCM bias configuration after removing the transformer. The final answer confirms that the AD9467 is optimized for differential inputs, and single-ended drive in DC-coupled mode can degrade SNR and SINAD. The recommended solution is to configure the ADA4945-1 as a single-ended-to-differential converter to ensure optimal performance. Key references include Analog Devices' articles on high-speed analog signal chains and differential ADC drivers.
AI Generated Content
Category: Hardware
Product Number: AD9467

Hi everyone,
I’m working with the AD9467-FMC-250EBZ board and need clarification on whether my modified input topology is electrically correct or fundamentally incompatible with the AD9467 analog front end.

Goal

I want to feed the ADC with a DC-coupled signal from an external amplifier instead of the default AC-coupled transformer network.

What I Changed

  • Removed the transformer-based input section (T100/T101/T102/T104).

  • Replaced C109 and C110 with 0-Ω jumpers to allow DC coupling into VIN+ / VIN−.

  • Reinstalled the VCM bias network (R111, R112, C107) so VIN− can be held at the ADC’s ~2.15 V common-mode if needed.

  • Using ADA4945-1 as the external driver.

Two modes I tested

1. Differential Drive (OUT+ → VIN+, OUT− → VIN−)

This SHOULD be supported, but I am checking whether DC coupling is valid with the jumpers installed.

2. Single-Ended Drive Using VCM (OUT+ → VIN+, VIN− biased to VCM)

This is the topology I am uncertain about.

Problem Observed

In the single-ended mode:

  • The ADC output collapses to a flat line

  • Or produces unstable spikes/random vertical noise

  • As if the differential input stage cannot establish a valid common-mode reference

This happens even when R111/R112/C107 are installed correctly.

My Question (Main Point)

After removing the transformer, is it electrically supported to operate the AD9467 in a single-ended + VCM bias configuration where:

  • VIN+ receives the signal

  • VIN− is tied to VCM (via the onboard R111/R112/C107 network)

  • And only OUT+ from the ADA4945 is used?

Or…

Does the AD9467 absolutely require a true differential drive at both VIN+ and VIN− when operated in DC-coupled mode (transformer removed)?

Why I’m Asking

I am designing a custom signal-conditioning PCB using ADA4945-1.
Before I finalize the board, I need to know whether “Option C” (single-ended + VCM) is a valid input configuration, or if the ADC requires differential drive only.

Any confirmation, schematics, or official recommendation for DC-coupled operation would be extremely helpful.

Thanks in advance.

Parents Reply Children
No Data