Post Go back to editing

AD9467-FMC-250EBZ – Is DC-Coupled Single-Ended Drive Using VCM Bias Electrically Valid After Removing Transformer Stage?

Thread Summary

The user asks if the AD9467 ADC can be operated in a single-ended + VCM bias configuration after removing the transformer. The final answer confirms that the AD9467 is optimized for differential inputs, and single-ended drive in DC-coupled mode can degrade SNR and SINAD. The recommended solution is to configure the ADA4945-1 as a single-ended-to-differential converter to ensure optimal performance. Key references include Analog Devices' articles on high-speed analog signal chains and differential ADC drivers.
AI Generated Content
Category: Hardware
Product Number: AD9467

Hi everyone,
I’m working with the AD9467-FMC-250EBZ board and need clarification on whether my modified input topology is electrically correct or fundamentally incompatible with the AD9467 analog front end.

Goal

I want to feed the ADC with a DC-coupled signal from an external amplifier instead of the default AC-coupled transformer network.

What I Changed

  • Removed the transformer-based input section (T100/T101/T102/T104).

  • Replaced C109 and C110 with 0-Ω jumpers to allow DC coupling into VIN+ / VIN−.

  • Reinstalled the VCM bias network (R111, R112, C107) so VIN− can be held at the ADC’s ~2.15 V common-mode if needed.

  • Using ADA4945-1 as the external driver.

Two modes I tested

1. Differential Drive (OUT+ → VIN+, OUT− → VIN−)

This SHOULD be supported, but I am checking whether DC coupling is valid with the jumpers installed.

2. Single-Ended Drive Using VCM (OUT+ → VIN+, VIN− biased to VCM)

This is the topology I am uncertain about.

Problem Observed

In the single-ended mode:

  • The ADC output collapses to a flat line

  • Or produces unstable spikes/random vertical noise

  • As if the differential input stage cannot establish a valid common-mode reference

This happens even when R111/R112/C107 are installed correctly.

My Question (Main Point)

After removing the transformer, is it electrically supported to operate the AD9467 in a single-ended + VCM bias configuration where:

  • VIN+ receives the signal

  • VIN− is tied to VCM (via the onboard R111/R112/C107 network)

  • And only OUT+ from the ADA4945 is used?

Or…

Does the AD9467 absolutely require a true differential drive at both VIN+ and VIN− when operated in DC-coupled mode (transformer removed)?

Why I’m Asking

I am designing a custom signal-conditioning PCB using ADA4945-1.
Before I finalize the board, I need to know whether “Option C” (single-ended + VCM) is a valid input configuration, or if the ADC requires differential drive only.

Any confirmation, schematics, or official recommendation for DC-coupled operation would be extremely helpful.

Thanks in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.