Post Go back to editing

CML (Current-Mode Logic) clock for AD9695

Thread Summary

The user asks if CML can be used for Sysref & CLK on the AD9695, despite Table 4 listing only LVDS and LVPECL. The final answer confirms CML can be used with proper termination and biasing to meet input specifications. For the Sysref path (750KHz), DC coupling is recommended if voltage levels are compatible; otherwise, AC coupling is acceptable but introduces a high-pass filter.
AI Generated Content
Category: Hardware
Product Number: AD9695

I have two questions.

1)Can the CML clock be used for Sysref & CLK?

It is mentioned in Figure 78 on page 31.

In Table 4, only LVDS and LVPCEL are mentioned. Why is there a contradiction in the data sheet?

2)Should the Sysref path be DC coupled? Sysref frequency=750KHZ

Parents
  • Hi  

    Thanks for your interest in AD9695.

    1. CML can be used, but proper termination and biasing are required to meet the AD9695 input specifications (similar to LVPECL). The apparent contradiction isn’t actually one: Table 4 lists the officially supported standards, while the figure illustrates the input structure, which can accommodate other differential types if correctly adapted. When using CML, ensure the input common-mode voltage and swing are within specification.
    2. For one-shot or continuous SYSREF, DC coupling is recommended when the driver and receiver share compatible voltage levels (e.g., LVPECL or LVDS at the same I/O voltage). If levels differ, AC coupling is acceptable but note that AC coupling introduces a high-pass filter.

    Please note that I’m not the official product owner, and these are just my comments. Kindly give some time for the product owner ( ) to look into this and provide their response.

Reply
  • Hi  

    Thanks for your interest in AD9695.

    1. CML can be used, but proper termination and biasing are required to meet the AD9695 input specifications (similar to LVPECL). The apparent contradiction isn’t actually one: Table 4 lists the officially supported standards, while the figure illustrates the input structure, which can accommodate other differential types if correctly adapted. When using CML, ensure the input common-mode voltage and swing are within specification.
    2. For one-shot or continuous SYSREF, DC coupling is recommended when the driver and receiver share compatible voltage levels (e.g., LVPECL or LVDS at the same I/O voltage). If levels differ, AC coupling is acceptable but note that AC coupling introduces a high-pass filter.

    Please note that I’m not the official product owner, and these are just my comments. Kindly give some time for the product owner ( ) to look into this and provide their response.

Children
No Data