Post Go back to editing

ADC code variations with Power cycle

Thread Summary

The user is experiencing significant readback errors (>50mV) with the AD9681 ADC after power cycles, which affects precision measurements. The final answer suggests using a low-jitter clock source, setting VCM to AVDD/2, decoupling VREF with specific capacitors, and issuing a digital reset via Register 0x08 to minimize variations. Additional steps include reconfiguring the ADC via SPI after each power cycle to ensure consistent settings.
AI Generated Content
Category: Hardware
Product Number: AD9681

Hi ADI team,

We are using AD9681 ADC in our application for V and I precision measurements.

However this ADC is changing the code with power cycle for upto 30 codes from lower input to Full scale input, which is causing significant readback errors of >50mV.

Since our product is required to meet high precision with 5mV in full scale input, we cannot compromise this.

We are applying code correction and calibration to mitigate errors. However power cycle to power cycle variations are not resolving with calibration.

Could you please let us know if this can be fixed?

Parents
    •  Analog Employees 
    •  Super User 
    on Nov 17, 2025 1:23 AM Contains AI Generated Content
    0

    Hi  

    Thank you for using AD9681.

    The AD9681 is optimized for high-speed data conversion, supporting rates up to 125 MSPS, with excellent dynamic performance and low power in space-constrained applications. It provides 14-bit resolution with typical DNL of ±0.8 LSB and INL of ±1.2 LSB, ensuring good linearity and accuracy. However, the device does not include an internal mechanism to guarantee identical code mapping across power cycles without external calibration, and it is not characterized for high precision measurement.

    To help minimize variation, please consider the following steps:

    • Clock Source Stability: Use a low-jitter, crystal-controlled clock source to maintain stability during power-up and operation.
    • Analog Input Configuration: Set the common-mode voltage (VCM) to AVDD/2 for optimal ADC performance.
    • Reference Voltage Decoupling: Decouple VREF to ground with a 0.1 µF ceramic capacitor and a 1.0 µF low-ESR capacitor to ensure a stable reference voltage.
    • Digital Reset: After the clock is stable, issue a digital reset using Register 0x08 to reinitialize the device correctly and reduce power-cycle variations.
    • SPI Configuration: If the issue persists, reconfigure the ADC via SPI after each power cycle to verify all settings are correct and consistent.
Reply
    •  Analog Employees 
    •  Super User 
    on Nov 17, 2025 1:23 AM Contains AI Generated Content
    0

    Hi  

    Thank you for using AD9681.

    The AD9681 is optimized for high-speed data conversion, supporting rates up to 125 MSPS, with excellent dynamic performance and low power in space-constrained applications. It provides 14-bit resolution with typical DNL of ±0.8 LSB and INL of ±1.2 LSB, ensuring good linearity and accuracy. However, the device does not include an internal mechanism to guarantee identical code mapping across power cycles without external calibration, and it is not characterized for high precision measurement.

    To help minimize variation, please consider the following steps:

    • Clock Source Stability: Use a low-jitter, crystal-controlled clock source to maintain stability during power-up and operation.
    • Analog Input Configuration: Set the common-mode voltage (VCM) to AVDD/2 for optimal ADC performance.
    • Reference Voltage Decoupling: Decouple VREF to ground with a 0.1 µF ceramic capacitor and a 1.0 µF low-ESR capacitor to ensure a stable reference voltage.
    • Digital Reset: After the clock is stable, issue a digital reset using Register 0x08 to reinitialize the device correctly and reduce power-cycle variations.
    • SPI Configuration: If the issue persists, reconfigure the ADC via SPI after each power cycle to verify all settings are correct and consistent.
Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.