Post Go back to editing

ADC implementation with fpga

Thread Summary

The user needs to send a 40 MSPS 4-channel signal to a ZedBoard Zynq 7000 FPGA. The AD9219-65EBZ board can be used, but requires a custom interposer or adapter board to connect its LVDS outputs and SPI control signals to the FPGA. Ensure matched trace lengths and compatible I/O voltage levels, using level shifters if necessary.
AI Generated Content
Category: Hardware
Product Number: AD9219-65EBZ, AD9219, AD9219, AD9219, AD9219

I need to send a total of 40 MSPS 4-channel signal to the FPGA. For this, is it more reasonable to use the AD9219-65EBZ board or should I design a custom PCB for the AD9219 chip? I am more in favor of using the AD9219-65EBZ, but how can I make the physical connections between them? The FPGA I will use is ZedBoard Zynq 7000.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.