Post Go back to editing

AD9262 ADC output stuck at constant value

Thread Summary

The user reports that the AD9262 ADC outputs a constant value after power cycling. The final solution involves performing a software reset via SPI by writing to Register 0x00, ensuring clock stability during power-up, and checking the Overrange Detection configuration. Additionally, the user found that the power-down and reinitialization via SPI only works when Channel Index (Register 0x05) is set to 3, not 0 as described in the datasheet.
AI Generated Content
Category: Hardware
Product Number: AD9262

AD9262 after power cycling sometimes the ADC result is a constant value independent of the input.

Does anyone have a reset sequence for this problem? (RST pin is set to ground by PCB)

Thread Notes

Parents Reply Children
No Data