Post Go back to editing

Feasibility and Reference Design for Dual AD9250 with Kria SOM FPGA

Thread Summary

The user inquires about interfacing two AD9250 ADCs with the Kria SOM FPGA platform. The final answer confirms the feasibility, noting that the AD9250 uses the JESD204B interface, which is supported by Xilinx FPGAs. Reference designs for similar Xilinx platforms (KC705, VC707, ZC706) can be adapted for Kria. The AD9250 Evaluation Board and ADC-FMC Interposer Xilinx Reference Design are recommended for more details.
AI Generated Content
Category: Hardware
Product Number: AD9250

Hello,

We are in the early stages of a project and are considering interfacing two AD9250 ADCs with the Kria SOM FPGA platform.

First, I would like to check the feasibility of this setup. Has anyone successfully interfaced dual AD9250s with the Kria SOM or a similar FPGA?

Second, if this is feasible, are there any available reference designs—both HDL and Linux drivers—that we could use as a starting point?

Any advice or shared experience would be greatly appreciated.

Thank you!

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.