Post Go back to editing

issue in writing to register of ADC

Category: Hardware
Product Number: AD8285

Hi Team,

I am currently working on interfacing with the AD8285 using a Blackfin processor. During my testing, I observed an issue when attempting to read and write to the device. Specifically, when I attempt to read the default address (0x01), I am able to retrieve the expected values from the register. However, when I write to the register and then attempt to read it back, I consistently receive a value of 0x00, regardless of the data written.

I am unsure where the value might be getting reset or what could be causing this issue. Could anyone please provide guidance on potential causes for this behavior or any suggestions on how to troubleshoot the issue.

I'm configuring the ADC through SPO0 line with sel1 in which, during write I'm able to see the data dump through the scoping.

I have checked the waveform in scope in which cmd, address, values are going correctly x20, x1A, xDE, xAD.
Also for ref I have provided the codes in which I have been configuring and read & write is happing.

uint8_t readPointer[16]    = {0x00, 0x00, 0x01, 0xA0};
uint8_t ADC = 0u;

if(spi_init(ADC) != API_SPI_SUCCESS)
 {
 perror("ADC init failed!.\n");
 }

 if(spi_ADC_cfg(ADC, clock) != API_SPI_ADC_CFG_SUCCESS)
 {
 perror("ADC CFG failed!.\n");
 }

// 0xDE, 0xAD
 spi_readwrite(ADC, &readPointer[0], 4);

 readPointer[0] = 0x00;
 readPointer[1] = 0xDA;
 readPointer[2] = 0x1A;
 readPointer[3] = 0x20;

 spi_readwrite(ADC, &readPointer[0], 4);

 for(int i=0;i<1000000;i++)
 {;}

 readPointer[0] = 0x00;
 readPointer[1] = 0x00;
 readPointer[2] = 0x1A;
 readPointer[3] = 0xA0;
 spi_readwrite(ADC, &readPointer[0], 4);

//and function defintions

 

static API_SPI_DEVICE gdevice[] = {{}}; // Global device handler and pointer
static uint8_t gmem[ADI_SPI_INT_MEMORY_SIZE]; // Global use memory

/static uint8_t gpointer[ADC_POINTER] = {0x00, 0x00, 0x01, 0xA0}; // D1, D0, Address, command
static uint8_t readPointer[ADC_POINTER] = {0};

API_SPI_RESULT spi_init(uint8_t device_id)
{
API_SPI_DEVICE *pDevice = &gdevice[device_id];
pDevice->device_id = device_id;
pDevice->instance = true;

if (pDevice->instance != true)
{
return API_SPI_INIT_FAILURE;
}

return API_SPI_SUCCESS;
}

 

API_SPI_RESULT spi_ADC_cfg(uint8_t device_id, uint16_t clock)
{
API_SPI_DEVICE *pDevice = &gdevice[device_id];

if(pDevice->instance == true)
{

pDevice->device_cfg.clock = clock;
pDevice->device_cfg.data_cfg.pTransmitter = NULL;
pDevice->device_cfg.data_cfg.TransmitterBytes = 0;
pDevice->device_cfg.data_cfg.pReceiver = NULL;
pDevice->device_cfg.data_cfg.ReceiverBytes = 0;
pDevice->device_cfg.dTransfer_Complete = false;
adi_spi_Open(pDevice->device_id, &gmem, ADI_SPI_INT_MEMORY_SIZE, &pDevice->handle);

adi_spi_SetMaster(pDevice->handle, true); // MSB
adi_spi_SetLsbFirst(pDevice->handle, false);
adi_spi_SetHwSlaveSelect(pDevice->handle, false);
adi_spi_SetClock(pDevice->handle, pDevice->device_cfg.clock);
adi_spi_SetTransmitUnderflow(pDevice->handle, false);
adi_spi_SetClockPhase(pDevice->handle, true);
adi_spi_SetClockPolarity(pDevice->handle, false);
adi_spi_SetWordSize(pDevice->handle, ADI_SPI_TRANSFER_32BIT); // if size needs to be large you can use 16bit or 32bit
adi_spi_SetTxWatermark(pDevice->handle, ADI_SPI_WATERMARK_50, ADI_SPI_WATERMARK_DISABLE, ADI_SPI_WATERMARK_DISABLE);
adi_spi_SetRxWatermark(pDevice->handle, ADI_SPI_WATERMARK_50, ADI_SPI_WATERMARK_DISABLE, ADI_SPI_WATERMARK_DISABLE);
adi_spi_SetSlaveSelect(pDevice->handle, ADI_SPI_SSEL_ENABLE1);
adi_spi_RegisterCallback(pDevice->handle, SpiCallback_Master, (void*)pDevice);

return API_SPI_ADC_CFG_SUCCESS;
}

/else
{
return API_SPI_ADC_CFG_FAILURE;
}
}

 

API_SPI_RESULT spi_readwrite(uint8_t device_id, uint8_t *data, uint32_t data_size)
{

API_SPI_DEVICE *pDevice = &gdevice[device_id];

pDevice->device_cfg.data_cfg.pTransmitter = data;
pDevice->device_cfg.data_cfg.TransmitterBytes = data_size;
pDevice->device_cfg.data_cfg.pReceiver = readPointer;
pDevice->device_cfg.data_cfg.ReceiverBytes = data_size;

adi_spi_SubmitBuffer(pDevice->handle, &pDevice->device_cfg.data_cfg);

while (!pDevice->device_cfg.dTransfer_Complete); // used for transmitting the whole data

pDevice->device_cfg.dTransfer_Complete = false;

printf("Receiver print --> 0x%02x\n",readPointer[0]);
printf("Receiver print --> 0x%02x\n",readPointer[1]);
printf("Receiver print --> 0x%02x\n",readPointer[2]);
printf("Receiver print --> 0x%02x\n\n",readPointer[3]);

return API_SPI_RW_SUCCESS;
}

 

void SpiCallback_Master(void* pHandle, uint32_t u32Arg, void* pArg)
{
API_SPI_DEVICE *pDevice = (API_SPI_DEVICE *)pHandle;
ADI_SPI_EVENT event = (ADI_SPI_EVENT)u32Arg;

switch (event) {
case ADI_SPI_TRANSCEIVER_PROCESSED:
pDevice->device_cfg.dTransfer_Complete = true;
break;
default:
break;
}
}



If I'm not wrong for reading to happen we have to send w/r, w0, w1, address in which my case A0, 0, 1, 0x01 where I'm able to read data correctly in half the cyclic
undefined

but when I change the bit 10100000 to first bit to be toggled to low for writing, I'm unable to get any data in read cyclic.


As you can see in the middle part where first two peaks represents the 20 and next represents the address but other half seems to be empty.

for your reference I have also attached write cyclic below.
undefined

could you please help me on this I dont know, where I'm messing out.

Regards,
MOVAS

Parents Reply Children