Post Go back to editing

External reference of AD9650

Thread Summary

The user asked about the input voltage range for the external reference of the AD9650 ADC. The final answer clarifies that while the VREF pin can tolerate voltages from -0.3 V to AVDD + 0.2 V (2.2 V with AVDD at 2.0 V), the functional external reference input range is 0 V to 1.35 V, corresponding to a 2.7 Vpp full-scale input range. Using an external reference can improve gain accuracy and thermal stability.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9650

Hello.

I have a questoin about AD9650.

Is the input voltage range of the AD9650 external reference 0V to 1.35V?
In Table.11 of the datasheet, it is N/A.

Best regards.

  • Hi  

    Thanks for your interest in AD9650.

    The "N/A" entry in Table 11 likely indicates that the exact voltage range for the external reference input is not explicitly defined in that table. However, based on the absolute maximum ratings, the external VREF pin can tolerate voltages from –0.3 V to AVDD + 0.2 V, which equates to 2.2 V when AVDD is 2.0 V.

    Functionally, though, the ADC is designed to support reference voltages up to 1.35 V, which corresponds to a 2.7 Vpp full-scale input range. Therefore, the effective external reference input range is 0 V to 1.35 V, and the ADC input range scales as twice the VREF voltage.

    Additionally, the use of an external reference may help improve the ADC’s gain accuracy and thermal stability.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.