Hi
I want to know what the input noise of the EVAL-AD9248.
Thanks
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 4 hours |
JAlipio |
Closed |
AD9248
Production
The AD9248 is a dual, 3 V, 14-bit, 20/40/65 MSPS analog to digital converter. It features dual high performance sample-and-hold amplifiers and an integrated...
Datasheet
AD9248 on Analog.com
Hi
I want to know what the input noise of the EVAL-AD9248.
Thanks
Hello,
With the input of the evaluation board terminated with 50 ohms, one should be able to match the datasheet results shown below after capturing a large record of samples (>16 K) and calculating the rms value of the data set. 
Thank you very much
Thank you very much