Post Go back to editing

EVAL-AD9083 & ADS8-V3EBZ : The operation of the evaluation board is unstable.

Thread Summary

The user is experiencing inconsistent startup of the EVAL-AD9083 when used with the ADS8-V3EBZ evaluation board. The 12V FMC supply LED lights up briefly but then goes out, preventing normal operation. The final answer suggests checking the 12V supply, the Power Monitor ADM1178-1ARMZ, and the MOSFET gate voltage, as well as measuring current through R338 and inspecting for intermittent solder connections or short circuits. The user confirmed the issue occurs upon turning on the ADS8-V3EBZ and has reinstalled the ACE software and drivers.
AI Generated Content
Category: Hardware
Product Number: AD9083

Hi,

I'm DFAE. I have a question from my customer. 

My customer is evaluating the AD9083 using EVAL-AD9083 and ADS8-V3EBZ. However, after powering on and starting up the ADS8-V3EBZ, when trying to operate the EVAL-AD9083 from the GUI, the LED on the EVAL-AD9083 lights up once or twice, then goes out and stops working. If you repeat the same thing several dozen times, the LED on the EVAL-AD9083 may stay on and it may operate normally.

Once it operates normally, it will continue to operate normally unless the power is turned off. But, if the power is turned off, it will not start normally again.

The AC power supply that came with the evaluation kit is used as the power supply. The latest GUI, etc. are downloaded from the web and used.

What could be the reason why it rarely operates normally? Also, are there any ways to improve this?

Best Regards,

Akira

Thread Notes

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.