The AD9653 data sheet provides the functionality of SYNC

When I want to use the functionality of sync next only,how do I configure this register?2'b10 or 2'b11? expecting a reply,thanks.
AD9653
Recommended for New Designs
The AD9653 is a quad, 16-bit, 125 MSPS analog-to-digital converter
(ADC) with an on-chip sample-and-hold circuit
designed for low cost, low power, small...
Datasheet
AD9653 on Analog.com
The AD9653 data sheet provides the functionality of SYNC

When I want to use the functionality of sync next only,how do I configure this register?2'b10 or 2'b11? expecting a reply,thanks.
Hi CS1998
Thanks for using AD9653.
Multichip synch functionality is discussed in the Input Clock Divider section on page 26 of the datasheet.

Do also note that if you want to use the sync function, the clock divide in register address 0x0B should not be set to default (0x00).
If you will not use the clock frequency divider and provide the same sample clock for the multiple AD9253, all ADCs will be synchronized even without the SYNC pin.
Hi CS1998
Thanks for using AD9653.
Multichip synch functionality is discussed in the Input Clock Divider section on page 26 of the datasheet.

Do also note that if you want to use the sync function, the clock divide in register address 0x0B should not be set to default (0x00).
If you will not use the clock frequency divider and provide the same sample clock for the multiple AD9253, all ADCs will be synchronized even without the SYNC pin.
thanks for answer, another question: if I want to use the functionality of sync next only,how do I configure the register 0x109?2'b10 or 2'b11?
If you want to use Sync Next Only, 0x109 should be 0x02.
When 0x109 is set to 0x01, clock dividers will be reset to its initial state every time there is a sync pulse.
While if 0x109 = 0x02, resynchronization will happen only on the first sync pulse after the register is written.
Also note that you'll need to satisfy the setup and hold time requirements of the sync pulse with respect to the clock signal, as shown in Table 5 and Table 7 of the datasheet.
ok, thans