AD9208
Recommended for New Designs
The AD9208 is a dual, 14-bit, 3 GSPS analog-to-digital converter (ADC). The device has an on-chip buffer and a sample-and-
hold circuit designed for low...
Datasheet
AD9208 on Analog.com
HI
There has been a lot of discussion and talk about how to align data and clock lines in JESD circuits. But the result is not very clear
Lane rate=10Gbps
sample rate=1Ghz
What I have understood is as follows:
1)According to the JESD204B Survival Guide, the DEVICE CLOCK lines are the same length as each other & the SYSREF CLOCK lines are the same length as each other. And the DEVICE CLOCK lines should be shorter than the SYSREF CLOCK lines.
DCLK trace length <SYSREF trace length < DCLK trace length + 1 inch
2) the DEVICE CLOCK & CORE CLOCK & REFERENCE CLOCK lines are the same length as each other.
3)JESD lines in ADC1 which consists of 8 lanes, can be the same length or have a slight deviation in length from each other, which is about 4 mm in my board. And in JESD lines, we are not allowed to use the accordion method for the same length on the PCB.jesd204b structure is okay with a slight length deviation.
4)JESD lines in ADC2 which consists of 8 lanes, can be the same length or have a slight deviation in length from each other, which is about 4 mm in my board. And in JESD lines, we are not allowed to use the accordion method for the same length on the PCB.jesd204b structure is okay with a slight length deviation.
5)The jesd lines of each ADC do not need to be the same length as the other ADC.
6)The SYNC lines of both ADCs must be the same length.
Is my view correct?

Hi OHBsystemag
Kindly give time for the product owner (s.ilke ) to look into this and provide their response.
Although, I'm not an expert in JESD, this is what I think:
Also note that the minimum sample rate of AD9208 is 2.5 GSPS.

You can also want to check out other ADC below:
Hi OHBsystemag
Kindly give time for the product owner (s.ilke ) to look into this and provide their response.
Although, I'm not an expert in JESD, this is what I think:
Also note that the minimum sample rate of AD9208 is 2.5 GSPS.

You can also want to check out other ADC below:
Thank you