I set the input of AD9251 to VCM, the output should be all 0, but D0B-D4B are not 0。
The Vp-p of AVDD and DRVDD are all 15mV。
How can I get all 0 output ?
Thanks!

AD9251
Production
The AD9251 is a monolithic, dual-channel, 1.8 V supply, 14-bit, 20 MSPS/40 MSPS/65 MSPS/80 MSPS analog-to-digital converter (ADC). It features a high performance...
Datasheet
AD9251 on Analog.com
I set the input of AD9251 to VCM, the output should be all 0, but D0B-D4B are not 0。
The Vp-p of AVDD and DRVDD are all 15mV。
How can I get all 0 output ?
Thanks!

Hi oldcong
Thanks for using AD9251.
Here are a few things you can check:


Hi JAlipio
Thank you for your reply.
Here is my clock circuit . I use a LVDS clock to drive a AD9513 , the output of AD9513 drive AD9251.

Other circuits are same with your reply. I should do something to reduce power noise.
Hello,
The datasheet provides grounded histogram plot as shown below which represents the thermal noise contribution from the ADC core when its inputs are essentially shorted to each other. Since the 14-bit ADC's SNR is slightly better than 74 dBFS (i.e. 74.5 dBFS), its noise floor is about equal to a 12-bit ideal ADC where its thermal noise dominates since no signal is present (hence jitter from clock is not an issue for this test). The histogram below should that the distribution has about 1.1 LSB RMS noise since the SNR under low-signal conditions of the ADC is around 74.5 dBFS.
In your shown circuit........suggest that you short the inputs of your VINA and VINB as shown below to determine if your recorded histogram has similar RMS value. If it does............eliminate short and reconnect as normal to see how much degradation occurs.

Thank you very much.